Hello Art,
The only advice I have to share is recommend a device which has higher throughput in TI factories.
Tlvm13620 and TPSM63602 is being manufactured on a larger wafer in comparison to than older-gen devices and will be ramping across TI recently…
Hello Dice-K,
Yes this is a typo.
TLVM13620 is the reduced feature set option of TPSM63602. It does not have adjustable slew rate. I will mark these datasheets to be corrected.
Hello Ernst,
You may be able to improve the emissions with additional input filtering (e.g. LC filter on the input) and/or slowing down the switch rise time (e.g. R10 resistor on the evaluation board).
Here is an application note to help you design an…
Part Number: TLVM13620 Other Parts Discussed in Thread: TLVM13640 , , TPSM63602 , TPSM63604 Hi,
Please let us know in case we will introduce these devices to our customers. About the package. Package of TLVM13620 / 30 are 30pin, but TLVM13640 / 60 are 20pin…
Part Number: TPSM63606 Other Parts Discussed in Thread: TPSM63602 Hi team,
The VCC pin has 1uF inside, but it says that 1uF is required outside. Is an external capacitor required for the VCC pin?
Best regards,