Part Number: TPSM63606 Tool/software: Hi. We've been using some TPSM63606 parts for reducing input voltage from typically 28V to output either 12V, 5V or 3V3 rails. However we have one application where we would actually need to use it with a 5V input…
Part Number: TLVM13660 Other Parts Discussed in Thread: TPSM63606 , Tool/software: Hi, I will change device from TPSM63606 to TLVM13660 because TLVM is much lower than TPSM. My use case is Vin is 24V and Vout is 5V (Iout 3A - 4A). So TLVM can work correctly…
Part Number: TPSM63606 Dear Specialists,
My customer is evaluating TPSM63606 and has a question.
I would be grateful if you could advise.
---
I have questions regarding voltage and vurrent rating of internal FET of TPSM63606 at power off.
Could…
Part Number: TPSM63606 Other Parts Discussed in Thread: TPS25981 Hello, I am planning on using the TPSM63606 DC/DC and would like to power on after TPS25981 eFUSE is enabled and the PG line is asserted. My voltage in is 12V and the output voltage from…
Part Number: TPSM63606 Tool/software: Hi ,
I want to use the P/N:TPSM63606 for one of my 12V/3A O/P Requirement. I want to know for the 12V O/P what is the minimum I/P Voltage is required. I have the Input DC source of 15V(if required i can bring upto…
Part Number: TPSM63603EVM Other Parts Discussed in Thread: TPSM63606 Tool/software: Dear Sir/Madam,
we have design and develop TPSM63606 circuit which provide +15V to +5V output but it is not working giving expected output +6.3V .
it is showing output…
Part Number: TPSM63606 Other Parts Discussed in Thread: LM61460-Q1 If Vin is set to 5V, what is the maximum output voltage?
We have a requirement to generate a 5V supply when Vin is in the range 5V to 22V.
Part Number: TPSM63606 Tool/software: Hi Team,
We are using the TPSM63606RDLR buck for our design,
Whether we need to provide the isolation for PGND and AGND?
Thanks in Advance,
Regards, Sathya Priya N
Part Number: TPSM63606 Tool/software: Hello,
I have two boards connect together via a 10 cm ribbon cable. The voltage (+3V3) from a TPSM63606 is running through this cable. I killed 3 TPSM63606 on three different boards when doing the following:
…