Part Number: TPSM63608 Other Parts Discussed in Thread: TPSM63610 When i tried to run the sumaltion for 1V8 @ 0.8A , 1MHz it doesnt allow the change in frequency. By default it is in 0.2MHZ.
Hi Meghla,
1. You can try out the TPSM63608 for this application Data sheet - 9.2.2 Design 2 – Inverting Buck-Boost Regulator with Negative Output Voltage Note - I have limited knowledge on power related products, I would request you to please…
Hi Cam,
Sorry for the confusion. We do not suggest to the synchronization function for TLVM13610. The revision of the datasheet will eliminate the words related to clock synchronization.
What we recommend is to use TPSM63608 if the customer wants to fulfil…
Hello,
Yes the TPSM63608 can support that application.
Please see attached WEBENCH Design simulation result
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=7B6E9AB6E334567F
Regards,
Jimmy
Hi Brian,
The upper end of the vout range usually comes from the combination of the fixed inductance used, max switching frequency of the device, and internal slope compensation parameters.
Here is an alternative whose Vout range goes beyond 16V.
https…
Other Parts Discussed in Thread: LM61495 , TPSM63608 , TPSM63610 , LM61480 I need one 15V -> -5V Regulator, where load current will be around 2.8 to 5A. at 75C ambient Temperature.
Kindly, suggest me some regulators either with integrated Inductor or integrated…