Part Number: TPSM82821 Hello,
My customer is having some issues with board bring up and wanted to double check that the parts are correct since the top side marking seems unusual. The datasheet verifies that GA1 is for TPSM828211SILR (1.2V fixed) and GA4…
Part Number: TPSM82821 Hi team,
The allowable number of reflow for this module device is 3 times, right?
I read below white paper and I think the FAQ's answer can be applied to this device as well.
https://www.ti.com/lit/ug/slib006a/slib006a.pdf …
Part Number: TPSM82821 Other Parts Discussed in Thread: TPSM82822 Hi team,
My customer wants to know ripple noise and output accuracy performance in power saving mode.
Do you have any data and capture to show such the performances?
Regards,
Takashi O…
Part Number: TPSM82821
Power modules group,
Our customer is using the TPSM828212 (the 1.8V fixed output version) of this part. They bought the parts from one of our distributors. The parts have the marking GA0CS, but the datasheet says the marking should…
Part Number: TPSM82821 Other Parts Discussed in Thread: TPSM82823 , Hi,
I ma looking for a replacement for Enpirion regulators EN5339QI and EP53A8LQI. Can anyone suggest any TI replacement for the same.
Technical requirements for each regulator is as below…
Part Number: TPSM82821 Hi,
We are considering using TPSM82821 to replace some enpirion parts that are EOL. The TPSM82821 has a max output capacitance of 47uF, which is similar to the enpirion EP53A8xQI max of 60uF. However, we also have additional capacitance…
Part Number: TPSM82821 Hi team,
For the fixed output versions, can customer use a resistor divider to adjust the output, say take a 1.8V and output 2.5V or 3.3V? From the diagram below, it seems we just need to pick low enough resistors to override the…
Part Number: TPSM82821 Hi team,
According to the datasheet, at least 6uA current is required in the voltage divider. Does it mean the current flow from VOUT to GND, correct? because the leakage current at FB is 0.01uA.
Additionally, is it no problem to…
Part Number: TPSM82821 Other Parts Discussed in Thread: LMZ30602 , TPSM82864A Hi team,
My customer is looking for a buck module in CT detector to replace EN6310QI.
The requirements are as below:
1. 5V input and 1.1V output.
2. Output current is 0.3A max…