Part Number: TPSM82822 Hi,
How is this part marking on these TPS parts (image below) supposed to be read. According to the data sheet from TI for part number TPSM828224SILR the part marking is supposed to be G94. The part I have is marked with a G914D…
Part Number: TPSM82822 Other Parts Discussed in Thread: TPS54218 We want to use TPSM82822 to supply cores of FPGAs and uP, and the total output capacitance could be around 500uF.
I have seen in the datasheet, that the maximum recommended output capacitance…
Part Number: TPSM82822
I am using the TPSM82822SILR in a new design. I use it to generate 1.9V, 3.3V and 4V. For the 4V supply I tried increasing the 100pF capacitor to 1.1nF. but it makes no difference
For all 3 supplies they are disabled when the input…
Part Number: TPSM82822 Other Parts Discussed in Thread: TPS53316 I see the maximum output capacitance for the subject device is 47uF.
We are looking for a 3.3V -> 0.85V / 2A solution that can support ~ 1200uF of bypass capacitance required for an FPGA…
Part Number: TPSM82822 Hello Experts, I have same question as follows, instead output voltage is 1.9V. Do you have any way to output 1.9V by fixed output voltage version? ---------------------------------------------------------------------------------…
Part Number: TPSM82822 Hello Guys,
Good day.
Our customer need the adjustable TPSM82822SILR but it is not available anywhere. To solve his problem for a 1.1V (which is not available as a fixed output type) output he needs some confirmation.
Can any of…
Part Number: TPSM82822 Hello team,
I designed two circuits with 1.2V and 1.8V output on the TPSM82822.
Please check and comment on the Schematic, BOM, WEBENCH report in the attached document.
Sep_14_2020_TPSM82822_1.2V_2A_Design_File_Shintomi.pdf
…
Part Number: TPSM82822 Hello team,
I found TPSM82822 reel width information at the Carrier pack material lookup doesn't agree with that of the D/S.
Could you please check which one is correct? (8mm or 5.4mm?)
Regards,
Itoh
Part Number: TPSM82822 Other Parts Discussed in Thread: TPSM82823 , Hi team,
Ask for your help to confirm.
Does the surface material of the parts of TPSM82822SIMLR or TPSM82823 contain metal?
My customer's designs pad according to SMT Rule will exceed…
Part Number: TPSM82822 Tool/software: WEBENCH® Design Tools Hello team,
I use TPSM82822 for FPGA I/O power supply. There are two types, 1.8V/1.5Amax and 1.03V/1.5Amax. Other FPGA power supplies are also designed with TI's TPSM. For other FPGA power…