Part Number: TPSM82864A Hi,
We use LTspice as our primary simulation tool. Could you please provide the unencrypted SPICE model for the [TPSM82864A]?
Thanks for your support.
Part Number: TPSM82864A Hello,
I want use TPSM82864A in the Forced PWM mode. I also want to set the output voltage using a resistive divider on the FB pin. Can you please confirm whether my schematic is correct for this?
Best regards
Buddika
Part Number: TPSM82864A I want to achieve this: - when starting up, the device are configured to output 3.3V by R87 205k ohm. - after start up, the pin, the pin vest/mode see 3.3V as logic high and enter forced pwm mode. I want to ask will the pull down…
Part Number: TPSM82864A Hello TI Support Team,
We are currently using MPS power modules in our project, but due to severe lead time issues, we are looking for TI alternatives.
Current Parts in Use:
MPS MPM54504GBS-T (Quad-Output / 20A Total…
Part Number: TPSM82864A Other Parts Discussed in Thread: TPSM82816 , TPS62870 , TPSM8287A06
Hi Team,
we are designing a DCDC for FPGA voltage rails 0.85V and 1.8V and want to use the TPSM82864AA0SRDJ device, but the load voltage rails have some…
Part Number: TPSM82864A Other Parts Discussed in Thread: TPSM82810 , TPSM82813 Tool/software: Hi.
I designed a 5V to 3.3V circuit using TPSM82864AA0HRDMR.
I have a problem with the 3.3V output waveform.
What should I check?
Best Regards
Part Number: TPSM82864A Other Parts Discussed in Thread: TPSM82810 , TPSM8287A06
Tool/software:
Dear Texas Instruments Support Team,
I am an engineer currently working on a design that includes the buck converter part number LTM4604AEV#PBF . I have…
Part Number: TPSM82864A Dear,
i ve some note about the land pattern example (RDM0023A)
i think in the datasheet an measure is missing. For the pins 1,7,12,18 the overall height or width is missing.
thanks
Part Number: TPSM82864A Other Parts Discussed in Thread: TPS82130 , TPSM82866 Tool/software: Hello, we are facing noise pickup on a new prototype board featuring several TI step-down switchers. We must generate several voltages in the 1V0 ... 3V3 range…
Part Number: TPSM82864A Hi,
Who the accuracy of the resistor at VSET/MODE pin influence on the TPSM82864A accuracy?
is the 1% resistor accuracy will make the same TPSM82864A accuracy as the 0.1% resistor accuracy?
regards
Zeev Gerber