Part Number: TPSM82864A Dear,
i ve some note about the land pattern example (RDM0023A)
i think in the datasheet an measure is missing. For the pins 1,7,12,18 the overall height or width is missing.
thanks
Part Number: TPSM82864A Dear specialists,
My customer wants to simulate TPS82864A with Webench.
The circuit was opened using the initial settings in WEBENCH.
When I try to select SIMULATE, the message "Simulation not enabled for this design" is displayed…
Part Number: TPSM82864A Other Parts Discussed in Thread: TPSM8287A06 I have a question about the TPSM82864 loop stability due to load capacitance. Section 9.2.2.2 of the TPSM82864A/6A datasheet states the following about the output capacitors.
The capacitor…
Part Number: TPSM82864A Hi,
In the section 7.3 in the datasheet there is a limitation on VIN falling ramp.
The falling slew rate of VIN should be limited if VIN goes below VUVLO - 10mV/us.
I have
What will happen if the ramp will be faster?
When VIN goes…
Part Number: TPSM82864A Is there any problem in adding a 1μH inductor to the Vout side of the TPSM82864A as a noise countermeasure at the output destination?
Also, are FB and VOS correct as shown below, not near the VOUT pin but near the tip of the…
Part Number: TPSM82864A Hi,
Who the accuracy of the resistor at VSET/MODE pin influence on the TPSM82864A accuracy?
is the 1% resistor accuracy will make the same TPSM82864A accuracy as the 0.1% resistor accuracy?
regards
Zeev Gerber
Part Number: TPSM82864A Hello,
The TPSM82864A datasheet shows different high-side and low-side current limits as shown below.
What is the current limit value of the TPSM82864A power module when the customer uses it?
Thank you.
Part Number: TPSM82864A Hello,
the TPSM82864A/6A data sheet states: The output discharge is active when the EN pin is set to a logic low and during thermal shutdown. The discharge is active down to an input voltage of 1.6 V (typical).
What happens regarding…
Part Number: TPSM82864A Other Parts Discussed in Thread: TPSM82810 Hi all
I want to design in the TPSM828664A. Datasheet states: "Values over 150uF can degrade loop stability of the converter."
Design is 5V input, 0.8V / 3.5A Output. I would place…
Part Number: TPSM82864A Other Parts Discussed in Thread: TPSM82866A , Hello,
a question regarding TPSM82864A / TPSM82866A.
Datasheet states for the VSET/MODE pin description: "... a low level selects power save mode operation.".
In fact it is…