Part Number: TPS62868 Other Parts Discussed in Thread: TPSM82864A , TPS62865 Hi,
According to datasheet, output voltage can be selected between two output voltage registers by the VID pin.
For TPS628680ARQY, the VSET/VID pin is connected to external…
Hello Prajesh,
thanks for reaching out in E2E.
The TPSM82810 is indeed a very similar device, which comes closest as an alternative.
If you don't need the adjustable soft start feature and a fix 1ms output ramp time are OK, then the TPSM82864A would…
Part Number: LMZ30604 Other Parts Discussed in Thread: TPSM82864A Hi,
My customer has the following requirements: Input voltage: 3.3V, output voltage: 0.9V, rated current: 4A, output voltage ripple :0.2% of Vout
My questions are:
1. Do we have a…
Part Number: TPSM82823 Other Parts Discussed in Thread: TPS82085 , TPSM82864A , TPSM82810 , TPSM82813 Hello,
The thermal resistance information found in the TPSM82823 datasheet is significantly higher than other products with similar specifications…
Other Parts Discussed in Thread: TPS53513 , TPSM82864A Some TI power regulators specify ambient temperature in Recommended Operating Conditions.
E.g. TPS53513 has -40~85C Ta in datasheet and WEBench tool doesn't allow a calculation above 85C. Although…
Part Number: PTH04070W Other Parts Discussed in Thread: TPSM82823A , TPSM82864A Hi Team
The product pth04070wad we purchased has two color marks, white and black.
Has the marking of the product been changed? Thanks
Best regards,
xiaoqing
Part Number: TPS84410 Other Parts Discussed in Thread: LMZ30604 , TPSM82864A Please let me know about internal Inductance value(μH) of TPS84410 (or LMZ30604).
In the past I post below E2E thread, but I lost Email history and could not contact now. …
Part Number: TPSM82810 Other Parts Discussed in Thread: TPSM82866A , TPSM82864A HI Team,
For TPSM82810, abs Tj-max in datasheet is 125C, but WEBench tool allows Tj to go 150C and thermal shutdown temp is 170C. I wonder if actual abs Tj-max of this part…
Part Number: LMZ30604 Other Parts Discussed in Thread: TPSM82866A , TPSM82864A , Dear Specialists,
My customer is considering LMZM30604 and has a question.
I would be grateful if you could advise.
---
I'd like to use multiple LMZ30604s.
According…
Part Number: LMZ30604 Other Parts Discussed in Thread: TPSM82866A , TPSM82864A , SN74HCS05 Dear Specialists,
Our customer has a question.
---
INH pin of LMZ30604 has Pull Up and Pull Down resistor in the device.
Could you please let us know the…