Part Number: TPSM82866C Deasr Sir/Madam,
TPSM82866CA3PRCFR is specified as "Software Enable Device = 1 (hardware enable)". The measing of this is unclear. It implies that CONTROL register bit 5 is always 1 and cannot be changed by IIC.
I am looking…
Part Number: TPSM82866C Other Parts Discussed in Thread: TS5A3157 Dear Sir/Madam,
For the TPSM82866CA3 when EN is low the IIC registers settings are cleared.
I am not sure why this decision was made.
If you could set the output voltage by IIC then…
Part Number: TPSM82866C Hello team,
Datasheet describes it can be used at A&D in the first page.
Is there additional radiation test for this device in order to apply A&D application?
Best Regards,
Austin
Part Number: TPSM82866C Other Parts Discussed in Thread: TPS544C26 , TPS542A50 , LMR36503 , TPSM365R3 Tool/software: Hello, in the TI product, I'm finding a programmable voltage regulator IC with an adjustable voltage of 0–5V for I2C, SPI, or UART interface…
Part Number: TPS62873 Other Parts Discussed in Thread: TPSM82866C Now I design the an optical module.
For the DSP power, I use TPS62873 and TPSM82866CA2.
The MCU IO is 1.8V. Do TPS62873 and TPSM82866CA2 I2C work at 1.8V?
The Vcc for TPS62873 and…
Part Number: TPS62827 Other Parts Discussed in Thread: TPS62868 , TPSM82866C Tool/software: Hi,
We want set 2 output voltage level 2.1V and 2.5V. We using N-MOS in parallel the resistor on FB pin, is it may have any side effect? thanks!
Part Number: TPS62871 Other Parts Discussed in Thread: TPSM8287A12 , TPSM82866C Tool/software: Hi Sir :
Regarding TPS62871, I have the following questions to ask. Also, please help check the schematic diagram in the attachment. The selected chip is…
Part Number: TPS62870 Other Parts Discussed in Thread: TPS62869 , TPSM82866C Tool/software: Hi,
We may using TPS62870 to using on Vout 1.2V and 1.8V condition.
How to optimization comp value in these two voltage?
I use wenbench tool but seem Rcomp…
Part Number: TPSM82866A Other Parts Discussed in Thread: TPSM82823A , , TPSM8287A06 , TPSM82866C Tool/software: Hi, could you clarify how the VOS pin should be connected and what its function is vs FB? Looking through the datasheets of a few similar part…
Part Number: LM21215A Other Parts Discussed in Thread: TPSM82866A , TPS62870 , TPSM82866C Tool/software: Hello,
My customer was using the LM21215AMHE-1 under the following conditions.
- INPUT : 5V, OUTPUT : 0.9V, LOAD : 6A
They designed the circuit…