Part Number: TPSM8287A10 I am using TI MPN PTH03060WAH in our products. However according to EOL information received, TPSM8287A10BBHRDWR, TPSM8287B30HAPVCHR are the substitutes.
I am not able to find datasheet for MPNs TPSM8287A10BBHRDWR, TPSM8287B30HAPVCHR…
Part Number: LMZ31704 Other Parts Discussed in Thread: TPS84621 , TPSM8287A10
Hi,
If I'm having a no-load condition while the regulator is enabled, how can I implement SENSE function? It is to be noted that I have connected the SENSE to the VOUT at…
Part Number: TPSM8287A10BAHEVM Other Parts Discussed in Thread: TPSM8287A10 , TPSM8287A15 , TPSM8287A12 Tool/software: Dear Sir/Madam,
Hello,
May I kindly request you if you can provide me the altium schematic, and / or altium library (schematic…
Part Number: TPS65216 Other Parts Discussed in Thread: TPSM8287A10 Tool/software: Hi Team
do we have any PMIC solution which integrated inductor inside IC like power module?
requirement :
Buck*4 output voltage 0.85V~3.3V current spec is 10A…
Part Number: TPS62871 Other Parts Discussed in Thread: TPSM8287A10 Tool/software: Could you teach as follows;
Target device: TPS62871Z0WRXSR
Are there any exposed conductors other than those in the device terminal shapes listed in the datasheet? As…
Part Number: TPSM82816 Other Parts Discussed in Thread: TPSM8287A06 , TPSM82866A , TPSM8287A12 , TPSM8287A10 Hello,
I have three question in blue below.
Design requirements:
Vin = 5 V
Vout = 3.3 V
I_LOAD max < 6 A
C_LOAD = large and application…