Part Number: TPSM843321 Hi,
We are looking into using TPSM843321 with a voltage output range from 4.5V to 10V. But we need some clarification before we proceed with evaluation of this component.
In the beginning of the datasheet for TPSM843321, it…
Part Number: TPSM843321 Hi team,
My customer is considering switching from a discrete DC-DC converter to a power module that offers better noise mitigation, and based on their requirements and cost constraints, the TPSM843321 is currently the top candidate…
Part Number: TPSM843321
Hi TIer
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1504357/tps54338-rt-sync-pin-voltage-limits-with-rc-circuit
Similar to this issue, could you please help check if the SYNC…
Part Number: TPSM843321 Dear Sirs and Madams,
We are considering using the TPSM843321.
Input voltage: +5V to +12V
Output voltage: +4.5V
We are considering dynamically switching between +5V and +12V input voltage.
This module has a maximum…
Part Number: TPSM843321 Other Parts Discussed in Thread: TPSM843521EVM Tool/software: Hi TIer
My customer would like use TPSM843321 to do IBB mode DCDC.
Input is +5V , output is -5V current is 0.01A - 0.1A.
Customer want test EVM . I see we only…
Part Number: TPSM843321 Other Parts Discussed in Thread: TPS62933
Dear Sirs and Madams,
The main reason we chose this module is that it states that the maximum duty cycle is 98%.
I would like to confirm the switching frequency of the TPSM843321…