Part Number: TPSM843B22 Hi sir,
My customer use TPSM843B22 EVM board to do the evaluation, the condition is:
Vin=12V
Vout=5V
Iout=15A
Pd=7W (Pin-Pout)
After 30mins, the Tc goes to 101degC. (Ambient is 25 degC)
As datasheet…
Part Number: TPSM843B22 Hi sir,
Power module device usually has load current vs temperature performance picture as below, but TPSM843B22 doesn't have in datasheet, coudl you pls kindly suggest and provide?
Thanks a lot!
Part Number: TPSM843B22 Manufacturers usually provide a graph showing the decrease in output current as a function of temperature. For this device family, I haven’t seen such data. Does this mean that the component is capable of delivering its maximum…
Part Number: TPSM843B22-A26-A22-CALC Other Parts Discussed in Thread: TPSM843B22 Hello,
I'm experiencing some problems when running simulations in Webench.
I've created a new project for P/N TPSM843B22RDGR and it was all fine until I tried to perform…
Part Number: TPSM843B22 Other Parts Discussed in Thread: TPS543B22 Tool/software: The datasheets says, Low impedance bypassing of 'VIN' pins to PGND is critical, so need to place 10-nF to 100-nF capacitor from each VIN to PGND as close as possible.
…
Part Number: TPSM843B22 Hello,
My customer requested TI's review of the circuit for the TPSM843B22.
Please review the customer's circuit below to ensure there are no problems.
Thank you.
Part Number: TPSM843B22 Other Parts Discussed in Thread: TPS563252 I NEED TO DESIGN POWER TREE TO MY POWER BOARD FOR THAT I USED TPSM843B22RDGR BUCK CONVERTER INPUT VOLTAGE IS 15V AND OUTPUT VOLTAGE IS 5V AND OUTPUT CURRENT IS 0.05 A
for that i need…
Part Number: TPSM843B22 Other Parts Discussed in Thread: TPSM843A26 , TPSM843A22 , I found the phase margin of the example circuit in 'TPSM843B22_TPSM843A26_TPSM843A22_Loop_Response' only be about 38deg. Do TI think this is a typical and acceptable value…
Part Number: TPSM843B22-A26-A22-CALC Other Parts Discussed in Thread: TPSM84538 , TPSM84338 , TPS54538 Hello,
Please ignore the TI Part number above "TPSM843B22-A26-A22-CALC" - we were unable to complete the form using the actual part number we are…
Part Number: TPSM843B22 HI
The design schematic diagram of TPSM843B22 is shown below. Could you please help check if there are any issues? Or good advice?