Part Number: TPSM84424 Hi all,
We're using the TPSM84424MOLR on one of our designs as a 1.8V regulator for many devices across the board. This is a >+30dBm output power RF based design and we see some switching noise spurs of the 1.8V regulator set…
Part Number: TPSM84424 Hi,
The specification of TPSM84424 mentions that its maximum input voltage is 17V and the absolute maximum rating is 19V.
If the input voltage is between 17V and 19V, will the IC have any protection action?
Part Number: TPSM84824 Other Parts Discussed in Thread: TPSM84624 , , TPSM84424
Hi support team,
According to the original question above, I think TPSM84824, TPSM84624, and TPSM84424 are the same device. Is the price difference due to different shipping…
Part Number: TPSM84424 Since TPSM84424 is a QFN Open Frame, Can components be places below the TPSM84424 module?
If yes what is the maximum height possible for such scenario?
Part Number: TPSM84424 Other Parts Discussed in Thread: TPS54824 , TPSM84624 , TPS54424 Hi is there a Power Monitor Sequencer for multiple TPSM84424. I am using a LTC2977 in current design, but looking for options for a new design. - Patrick
Part Number: TPSM84424 Hi,
Sequencing schematic/connection as shown in datasheet Fig22 on page 19 does not show any pull-up connection - Doesn't it requre a pull-up? Since the PGOOD pin will be open-drain/floating when Vout is good (>89% 0r <108% of…
Part Number: TPSM84424 Dear,
We ordered PN# TPSM84424MOLR (600 pcs) via ORDER# T00775303, so far, our customer has used 490 pcs, but there are 12 pcs among them got qualilty issue.
The balance 110 pcs on our hand, not to use just in case.
Failure…
Part Number: TPSM84424 Hi,
Regarding TPS84424 , DC/DC control block and other components are placed underneath the inductor. Is there any possibility that DC/DC control block is affected by leakage flux from the inductor? If there's no possibilities…
Part Number: TPSM84424 Other Parts Discussed in Thread: LMZ31704 Hi,
I'd like to know the reason TPSM84424 uses Open-Frame package.
Some previous generation power module which has similar spec (like LMZ31704) is using QFN.
What is the main benefit…
Part Number: TPSM84424 Other Parts Discussed in Thread: TPS82130 Hi Team,
My customer is making the Thermal evaluation,
We know we have shown the Tj Recommended Rating 105C in the datasheet, but how about the Tcase Recommended Rating ?
Can we provide…