Part Number: TPSM84A21 Good Morning,
Could you please confirm the plating on the pads in the termination area? If gold, are they ENIG or ENEPIG?
Thank you!
Part Number: TPSM84A21 Tool/software: Hi support team,
The PGOOD output of the TPSM84A21 is not stable.
When the feedback to VS+ was changed from the far end (81mm) to a closer point (51mm), the oscillation seemed to subside. Also, when a 47Ω resistor…
Part Number: TPSM84A21 Tool/software: We have a system with the TPSM84A21MOJRpart. We have the enable at 2.1V and 10V in. The Rset value is 732 ohms which should give 1.2V on the output. What we see is 0.618V on the output and the PG pin is low. If we…
Part Number: TPSM84A21 Hi team,
I would like to measure the loop response of TPSM84A21EVM.
There is R7(0 ohm) on the EVM, can I measure changing R7?
Is it possible to measure even if there is 10-ohm between VOUT and VS+ inside?
Best Regards…
Part Number: TPSM84A21 Other Parts Discussed in Thread: TPS54A20 Hi team,
The output has a ripple of tens of kHz. 12Vin 0.85Vout setting. The load has a total of 1300uF capacitors. Is it caused by the capacitance more than the data sheet recommended…
Part Number: TPSM84A21 Hello,
I have multiple regulators off a single 12V rail off a server. The switching freq of the 12V input is unknown and can vary from server to server. Are there any recommended input filter values for use with this regulator…
Part Number: TPSM84A21 Other Parts Discussed in Thread: TPS54824 Hi Team,
Our customer would like to use TPSM84A21 for Xilinx Zynq Ultra+ MPSoC XCZU7CG-1FFVC1156E. I have shared the link to the recommended voltage regulator IC for FPGA in the link below…