Part Number: TPSM861252 Hello team,
I think that the below figure has typo on Vin or Vout values. Can you check the data in your team and modify as needed?
*Ex) Figure 6-17: Vin=3.3V -> Vout=5V?
Best regards,
Shotaro
Part Number: TPSM861252 Hello team,
Can you help me to answer the below item?
<Package outline>
Does this value mean typical? If so, can you check min/max value for a reference?
<Example board layout>
What is the reason why TI recommend "Non…
Part Number: TPSM861252
Hi TI Expert,
We are using TPSM861252 to design a power supply with the spec. as below:
Vin: 4.5 ~ 12.5V
Vout: 3.3V
Ioutmax: 1A
In the datasheet(SLUSFD2B, Table 8-2) it is recommended RFB = 135k/30k, and Cff = 22pF…
Part Number: TPSM861252 Tool/software: Hi,
The unit of VOVP is %. Am I correct in understanding that this value is based on the output voltage set by the user? For example, if I set the output voltage to 3.3V using the FB resistor, is it correct that…
Part Number: TPSM861252 Other Parts Discussed in Thread: TPSM861253 Tool/software: Hello team,
Which is the best layout for RFBB and RFBT on TPSM861252?
(I think the EVM is based on TPSM861253. So the way on datasheet is the best. Is it correct?)…
Part Number: TPSM861252 Other Parts Discussed in Thread: TPSM863252 Tool/software: Hello,
Can you share the efficiency for this module at the following voltage rails?
Vin = 1.8V ; Vout = 1.0V @ 130A
Vin = 3.3V ; Vout = 2.5V @ 160A
Vin = 12V…