Part Number: TPSM863257 Other Parts Discussed in Thread: TPSM84624 , TPS51200 Tool/software: Please help to review attached schematics having parts:TPSM863257,TPSM84624,TPS51200,TPS7A8101QDRBR,TPS7A4901DRBR VVDN_Schematics_Power_design_SPIU_030724 (1)…
Part Number: TPSM863257
Hi team,
In datasheet, it is said that " Vias are optional depending on application, refer to device data sheet. If any vias are implemented".
In what case vias need to be opened? (For typical usage, do we need to open…
Part Number: TPSM863257 The Datasheet is showing thermal via´s also for the not connected SW pad.
Do we need them as heatpipes ?
Can we remove them ?
Do we need to add extra copper on different layer ?
Part Number: TPSM863257 Hi team,
About package, customer have two questions following. Could you support these?
Does the side face of pin 5to7 has conduction points? (same as side face of pin1&2 , 3&4)
Is it necessary to solder the electrodes…
Part Number: TPSM863257 Hi team,
From Fig 8-14. in datasheet, It is seems that EN drop and Vout drop are approximately same time when shutdown through EN.
Is there a delay time between EN low and Vout starts to fall? If it exists, how many seconds?
…
Part Number: TPSM863257 Hi,
Could you please send me the 3D CAD file for this part? I can see same question being asked in the forum, but I cant see a model released in the thread.
Cheers,
Kaushalya
Part Number: TPSM861252 Other Parts Discussed in Thread: TPSM863257 Tool/software: Hi,
I have a question about the PG (Power Good) pin of TPSM861252 and TPSM863257.
1) There was no description of Power Good on the data sheet. Could you give me the waveform…