Part Number: TPSM86837 Tool/software: Hello,
I have two devices of TPSM86837RCG in which initial operation was ok, but after several powerups the devices failed, they are not switching anymore, showing 125 & 160 ohm short to ground in the enable pin…
Part Number: TPSM86837
Official Purchase: TPSM86837RCGR
Current Usage Status: - Batch 2438: 350 units mounted, 150 units defective
- Batch 2507: 50 units mounted on March 22, 21 units defective as of now
Mounting Method: Reflow soldering, peak…
Part Number: TPSM86837 Tool/software: We are making a new electronic design and we need a DCDC module (Vin=24V, Vout=5V, Iout=6.5A-7A).
We are thinking about using the TPSM86837 module and we want to know if this component is going to have a long life…
Part Number: TPSM86837 Other Parts Discussed in Thread: TPSM86637 , TPSM86638 Tool/software: Someone asked this question about the TPSM86638 already, I just want to verify the same applies to the TPSM86637. Should the two SW pins be tied together on the…
Part Number: TPSM84538 Other Parts Discussed in Thread: TPSM843521 , TPSM86638 , TPSM86637 Hello,
I have a design where I need a 5V/3.5A output supply from 12V input voltage.
I found the TPSM84538 that would suite this application. In the datasheet…