Part Number: TRF370417 Other Parts Discussed in Thread: DAC38RF82 Hello RF Team,
Regarding TRF370417
The datasheet mentioned that this part supports an I/Q baseband input bandwidth of 1-GHz. With this bandwidth capability the input signal can be centered…
Part Number: TRF370417 Hi team,
Data only shows the 1db input freq bandwidth, what's the 3db input freq bandwidth?
Can we provide the input freq plot up to 2Ghz?
Thank you.
Part Number: TRF370417 Other Parts Discussed in Thread: TRF370317 , Hello
Couldn't find graph on the data sheet displaying OIP3 vs LO power. Do you have this data?
Also, I've noticed that the LO input is specified for LO power range -5dBm to +12dBm…
Hello Danny
Danny Racho said: The TRF needs a 1.7V common-mode at the input, or does the DAC already provides this voltage? For the DAC3152 is was the analog VCC, that set the output voltage. In the schematic I followed the trace of the output and just…
Part Number: DAC3484 Other Parts Discussed in Thread: DAC5688 , DAC3482 , DAC38J82 , DAC38J84 , TRF370417 , TRF3705 , Hello,
My customer is using the DAC5688 to receive I and Q input, up-convert them to complex NCO, and output one channel.
They are looking for…
Part Number: TRF370417 Other Parts Discussed in Thread: TINA-TI , Tool/software: TINA-TI or Spice Models Hi,
would like to check if there's SPICE model available for TRF370417? I can't seem to find it in SPICE model repository. Please advise. Thanks.…
Part Number: TRF370417 Hello ,
in the datasheet the part is defined from 50 MHZ to 6GHz , i would like to know the devices oppreation in frequacies less then 50 MHz
What would be the performence of the device ?
is there a graph of the degradation ?
Part Number: TRF370417 Dear Sirs: Related to an older thread (3 yrs ago) I am driving the LO port of the TRF 370417 from a synthesizer chip through a buffer amp. The input to the LO port is not a square wave as my frequencies on the LO port go from 600…
Part Number: TRF370417 Other Parts Discussed in Thread: DAC3484 , DAC38J84 , TRF3705 , DAC5687 , DAC5688 To whom it may concern,
According to the data sheet, TRF370417's two BB inputs have single-ended input impedance of 5kOhm.
I wonder if the differential…
Part Number: TRF370417 From my customer ...
Now we are facing noise floor issue of TRF370417. We tested the EVB of TRF370417 and found the test result worse than the value specified in datasheet. could you please check if our test condition and ways are…