Part Number: TRF371125EVM Tool/software: What is the Pre-Preg material and Stackup used for the TRF371125EVM? I am working on a board with 50 ohm traces and want to match the properties of the EVM board since it has low loss.
Part Number: TRF371125EVM I followed the instruction for the EVM test in the datasheet.
The current that the board runs is 290mA instead of 385mA in the datasheet.
When I checked using a spectrum analyzer, the mixer itself worked, but the BB amp did…
Part Number: TRF371125EVM What is the maximum voltage coming out of the BBIP, BBIN, BBQP, BBQN ?
Datasheet for TRF3711XX only says the DC common mode voltage, but no reference to max voltage swings of the baseband outputs.
Other Parts Discussed in Thread: TRF371125 , TSW3003
Hello,
I have 2 TRF371125 mixer eval boards that I am using in a system. I am using TI's provided software to program the two boards via USB, however, when I have both boards connected to…
Part Number: TRF371125 To whom it may concern:
Hello. I am designing my own board that has a TRF371125 on it. I followed the design of the TRF371125EVM for programming. I have USB and an FT245RL for programming. I am trying to use the labview code…
Other Parts Discussed in Thread: TRF371125EVM For indoor positioning we need a demodulator with a guaranteed propagation delay within 10ps accuracy ( delaymay be much longer as long as it is Always the same time).
Will the TRF371125EVM answer for our…
Other Parts Discussed in Thread: TRF371125EVM Hi, I'm Taeyeop.
I have a question about TRF371125EVM,
Now I'm using up-converter for TRF3702 and down-converter for TRF371125EVM. Both LO signals are divided by 2-way power divider of one signal generator…