Part Number: TRF3722EVM Other Parts Discussed in Thread: TRF3722 Hi,
I am trying to connect to TRF3722 EVM board over 4WI that the IC supports but I cannot find any information about pinout and how to connect to EVM board. Could you provide a datasheet…
Part Number: TRF3722EVM Other Parts Discussed in Thread: TRF3722 , TRF372017 , TRF3705 Hello,
I am trying to design a system using the TRF3722. I have a PCB in hand with our design, and have also evaluated the TRF3722 and TRF372017 using the EVM moduels…
Part Number: TRF3722 DEARS.
The VCC_TK of TRF3722EVM features 5V better than 3.3V. Is there data comparing VCC_TK 3.3V and 5V output? On the datasheet, all characteristics are measured with 5 V applied(Linearity(P1dB, OIP3), Phase Noise) Does TI recommend…
I’ve attached a plot of the worst case OIP3 for the TRF3722EVM. As the output power increases, the IM tones are higher in magnitude. In any case, the 1dB compression point is typically at 10.2 dBm for this device, so I would recommend staying below that…
Part Number: TRF3722 I am currently utilizing the TRF3722 in a transmitter design. While testing with the TRF3722EVM eval board (100MHz ref from a microwave source, 25 MHz PFD, and 2800 MHz output), I noticed what seemed like the reference frequency feeding…
Other Parts Discussed in Thread: TRF3722EVM , TRF3722 hello
I'am Alber as a FAE in Arrow Korea.
My customer tested the TRF3722EVM.
But there no has any signal intergrity on datasheet, such as Error vector Magnitude.
my customer measured the…
Part Number: TRF3722 Hi dear supporting team,
My customer uses TRF3722 in their product and they found several devices PLL might go unlock under cold temperature. After doing several tests, they found the unlock devices is related to 1911 batch.
We…
Other Parts Discussed in Thread: TRF3722EVM I downloaded the GUI for the TRF3722EVM, and it installed without complaint. When I plug in the EVM, Win 7 (64 bit pro) enumerates it as COM 8. When I click on the GUI, nothing happens except 3 processes show…
Other Parts Discussed in Thread: TRF3722EVM Figures 38-43 show the unadjusted carrier feed through (CF) for the TRF3722EVM evaluation module. Some of these figures show frequency bands of lower unadjusted CF performance such as:
Figure 38, typical…