Part Number: TRF7960A Hi,
We are evaluating the TRF7960A and have a few questions about the antenna layout for the SLOA135A.
1. Is the reason you recommend keeping the GND plane away from the antenna trace to avoid the effects of parasitic capacitance…
Part Number: TRF7960A Other Parts Discussed in Thread: TRF7960 , Dear Texas Instruments Support Team, We are currently using the TRF7960 for RFID communication and are attempting to retrieve a random number from an NXP ICODE SLIX2 tag using the ISO15693…
Part Number: TRF7960A Hi experts,
I would like to design the following feature using TRF7960A.
Could you recommend me an examples that I can refer to?
1) ISO/IEC 15693 Recognition of TAG IDs (including DSFID) 2) Recognition of Multi-TAG ID (including…
Part Number: TRF7960A Other Parts Discussed in Thread: TRF7970A Hi,
Could you please tell me whether the TRF7960A supports the following?
・ISO/IEC14443A MIFARE 1K 4K ・ISO/IEC14443A MIFARE UL AES ・ISO/IEC14443A MIFARE Plus ・ISO/IEC14443A MIFARE DESFire…
Part Number: TRF7960A Tool/software: I need to match the output network of a TRF7960A RFID IC, and I'm wondering in what state the IC should be in during matching. Should it be on or off? The datasheet has an example on matching it with an output impedance…
Part Number: TRF7960A Other Parts Discussed in Thread: TRF7970A , MSPM0L1306 , TRF7960 Tool/software: Hello, in the image bellow, you can see the connections of the TRF7960A on my board. The fact is that I am transmitting the REQA command for ISO14443A…
Part Number: TRF7960A Other Parts Discussed in Thread: MSPM0L1306 , SYSCONFIG Tool/software: Hello, I made a board based on TRF7960A reader, controlled by a MSPM0L1306 MCU, above, you can see the schematic of such board. For the coding, I want to go step…
Part Number: TRF7960 Tool/software: Hello
For a design in production we are unsing the TRF7960RHB and i see the TRF7960A.
Could you explain the difference between the TRF7960 and TRF7960A.
I find only the price, could you help me please?
The actual…
Part Number: TRF7960A Dear TI Experts,
We find tx impedance matching section in the datasheet, so we are curious that we don't seem to need to care about Rx matching. As we find input impedance of Rx is 10kohm (typ), partly we understand that we hope…
Part Number: TRF7960A Hi.
My client company requested a private design review of TRF7960A.
Please connect me to the technical representative of TRF7960A.
Regards,
thanks