Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: TRPGR30ATGB , TRPGR30ATGC , TRPGR30ATGA Dear all,
Our company focus on 300mm silicon wafer manufacture and we're looking for a type of 32mm RFID tag to be installed in a Fosb when silicon wafer shipping.
We're currently…
Can anyone confirm that the TRPGR30ATGC ( www.ti.com/.../trpgr30atgc) is supporting the requested anti-collision feature and can be used in combination with the MRD2EVM to read multiple TRPGR30ATGC tags in the same field?
Best regards,
Other Parts Discussed in Thread: TRPGR30ATGA , TRPGR30ATGB , TRPGR30ATGC , TRPGR30ENATGA , TRPGR30ENATGB Tech support sent me to this forum. Which of the following would be a suitable replacement to the part above:
TRPGP40TGC
TRPGR30ATGA
TRPGR30ATGB
TRPG…
Other Parts Discussed in Thread: TMS3705 , TRPGR30ATGC , TMS37157 Hello, I work with TMS3705 with TRPGR30ATGC. In my new application I want transponder coil separated of the electronic transponder. Texas have any transponder with this specification?
Hi Adam,
just take a look at the usual RFId key-Fob suppliers, they might have a standard housing they are offering and integrating 12 x 2.12mm and 23/32 x 3.85mm TI glass encapsulated tags, TRPGR30ATGC, TRPGR30ATGA, TRPGR30ATGB.
Regards,
KSA
Gilles -
I can see that Digikey has 1.6k in stock right now ==> www.digikey.com/.../en ;y=18&lang=en&site=us&keywords=TRPGR30ATGC
also, OregonRFID carries it ==> www.oregonrfid.com/index.php ;cPath=4&products_id=45
To add to Josh's comments:
R9WK, R9BK, W9WK are end-of-life. M9WK is soon to follow. So, please do not use any of those in a new design.
If you need wedge: TMS37145TEAIE is the right choice but it is not backward compatible.
If you need backward compatibility…
Other Parts Discussed in Thread: TRPGR30ATGC Dear all,
I now working with RI-TRP-R9BK products, but the poduction will stop next year. I need to replace it with a transponder with almost the same size and with the same ID address (compatibility with current…
Hi, we have some recapture of PIT tags, length 12 mm used on Salmo salar
http://www.ti.com/lit/ds/symlink/trpgr30atgc.pdf
ID:
985 170002014154
985 170002000609
Are these Texas instrument numbers and if so can you give us/customer information about…