Part Number: TRS3122E Other Parts Discussed in Thread: MAX3232 , , MAX3243 Hi team,
As title, is that OK to replace MAX3243 or MAX3232 with TRS3122E?
Customer would like to double check with the team, TRS3122E Dout with +-12V
Customer original design from…
Part Number: TRS3122E Hi,
1.Data rate support 1000kbps in the TRS3122E Datasheet(RL=3k ohm & CL=500pF) How should the circuit be added the RL and CL?
2.The transmission speed we currently use is 115200bps. Is there a limit on the transmission length…
Part Number: TRS3122E I have a question about the voltage translation, as the block shown below, the signal level from module board is 0V~5V, but the VCC and VL of TRS3122E is 1.8V, is it possible to damage TRS3122E ? can the TRS3122E works normal ?
Part Number: TRS3122E For dual-supply operation with Vcc = 3.3V and VL = 1.8V, do you recommend any capacitor selections be different than those shown in Table 1?
Part Number: TRS3122E Hi,
I would like to know if 10k ohm resistors used on the FORCEON and FORCEOFF_N in TRS3122E RS232 transceiver is fine. If not kindly suggest the value of the resistors to be used or will it be appropriate to not use the resistors…
Part Number: TRS3122E Other Parts Discussed in Thread: TRS3318E , Hi Team,
Quick question:
How would you recommend setting up TRS3122E for Vcc=2.5V? Looks like it falls in between the ideal ranges for doubler and tripler operation. Seems to me it will run…
Part Number: TRS3122E Team,
Our customer is using the TRS3122E, and to save more power, they'd like to force the TRS3122E into the auto-powerdown before 30 seconds of idle time is reached. They tried doing this with FORCEOFF, but this won't work,…
Part Number: TRS3122E
Hi,Sir:
For TRS3122E IC,configurate FORCEOFF# = HIGH and FORCEON = LOW to enable auto powerdown plus,
Both RINx,DOUTx,DINx,ROUTx signal could wake up the system?
Or just only DINx,RINx?
Or other cases?
Please also advice the…
Part Number: THVD4431 Other Parts Discussed in Thread: TRS3122E , THVD4421 , SN75155 , SN65C1168E , THVD1512 , SN65LVDS049 , THVD2410V Hello?
I'm currently considering an RS232 only transceiver. The conditions I'm looking for are as follows.
- Receiver…