Part Number: TRS3232E-Q1 So is the pin protected against 12V or not? If it is stated that the maximum allowable voltage is -6 +6, does that mean that the pin can withstand 12V if referenced to GND? And in an automotive design 12V is not enough because…
Part Number: TRS3232E-Q1 Other Parts Discussed in Thread: TRS3232 Hello team,
For TRS3232E-Q1, can you confirm if the following use case is okay?
The datasheet specifies Receiver input voltage up to 25V, so it’s expected that the different supply…
Part Number: TRS3232E-Q1 Hi Experts,
Can you please provide values for below parameters for the part TRS3232EQPWRQ1
Thermal Resistance Junction -to- Case
Thermal Resistance Junction-to-board
Thank you in advance. Kind regards, Gerald
Part Number: TRS3232E-Q1 Hi team,
How do we handle unused driver and receiver terminals? Is these pin floating OK? We need just 1ch line driver/receiver.
In addition, I understand TRS3232E-Q1 does not need any external amplifier on its each driver…
Part Number: TRS3232E-Q1 Hi
There is an error rate over 57,600 baud, the test waveform is below,Could you please help to analyze the possible causes?
Blue is the SCM output waveform
Yellow is the output waveform of the transceiver
The schematic…
Part Number: TRS3232E-Q1 Other Parts Discussed in Thread: TRS3232 I am doing a de-rating analysis on the TRS3232 RS232 line driver/receiver. What is the max voltage the caps see on V+(pin 2), V- (pin 6) and from pins 1 to 3 and 4 to 5?
Part Number: TRS3232E-Q1 Hi TI-team
My customer wants to use TRS3232E-Q1 in half duplex.
Can it be used with a half-duplex line ?
Please answer the following questions when available.
1.What should the peripheral circuit be ?
2.Is Pull Up…