Other Parts Discussed in Thread: TS12A4514 Hi,
My customer is looking for the analog switch like "TS12A4514 w/ Pulldown Register".
Do you know if TI has such kind of devices or similar devices?
Though I have been looking for, I have not found the…
There is a 32ns for start-up time and a 25ns turn off time. Since my pulses are in the 50ns range - I do not think I get proper output. I tried with a TS12A4514 , which has a similar pin-out and function. I think the start-up and turn-off times are too…
What should the output voltage be when the button is not pressed? Low, high, or floating?
You can use any 12 V switch for this, such as the CD4066B or TS12A4514.
If you use the unbuffered button signal, the bouncing can cause the switch to quickly…
As far as I can see, all analog switches have ESD protection diodes at the analog pins, i.e., the switched signal must not exceed V CC , or must be limited to a small current (but then the diodes would still clamp the signal).
Consider a device like…
Other Parts Discussed in Thread: SN74CB3Q3306A , SN74CB3Q3305 , TS12A4515 , TS12A4514 Hi,
Can you please confirm if INPUT of SN74CB3Q3305 or SN74CB3Q3306A is high Z when,
1) Vcc=0V
2) Vcc=3.3V but OE/=high (disabled)
I see only max Vcc level difference…
Sonia,
You can search for TI devices that are similar to competitor parts with the TI.com cross reference tool.
In addition to the TS12A4514 device TI has higher voltage product families such as the MUX509 and CD4016B.
To help narrow down…
Other Parts Discussed in Thread: TS12A4516 , TS12A12511 , TS12A4514 , TS5A9411 Hi, we are using TS12A4516 as a +-5.5V signal switch, the project is about to mass produce, we suddenly found out the TS12A4516's control logic high is VCC+ - 1.5V, however…
Frank,
The plot below is for the TS12A4515 but the TS12A4514, TS12A4515, TS12A4516, and TS12A4517 family of switches have very similar performance.
Thank you,
Adam
Kensuke-san,
The TS3USB221A datasheet states the following:
What is the signal voltage level and bandwidth you would like to switch? There may be better IC options if you only require a 1 channel SPST device like the TS3A4741, TS3A4742, TS12A4514…
Samir,
1) Based on the current consumptions it looks like the TS12A4514 and TS12A4515 likely have a CMOS transmission gate structure and the TS12A4516 and TS12A4517 likely have an nmos FET with a charge pump. What is driving the need for the architecture…