Part Number: TS3A27518E-Q1 Hi TI expert,
I would like to confirm whether below idea will work.
Since the IC act as a passive switch during on-state with certain ron.
With VCC up to 3.3V,
Could we bias NCx pins to 1.8V and NOx pins to 3.3V the using INx…
Part Number: TS3A27518E-Q1 Hi
I cannot find any propagation delay information in the TS3A27518E-Q1 datasheet.
What is the propagation delay through the TS3A27518E-Q1 (NCx/NOx to COM)?
Best regards, Martin
Hi,
Thank you for your suggestion, instead of the above multiplexers, can we use the below multiplexer? As we have 6 header pins, 3 for each DRVs. www.ti.com/.../TS3A27518E-Q1
Part Number: TS3A27518E-Q1 Our Application connects QSPI Flash Between the Processor and External Programmer through the TS3A27518E-Q1 Switch. The External Programmer is connected to NO and the Processor is connected to NC of the TS3A27518E-Q1 Switch.
…
Part Number: TS3A27518E-Q1 Other Parts Discussed in Thread: TS3A27518E , TMUX1574 Hello,
I need to make some simulations with a TS3A27518E using S parameters. I dowloaded them in this post https://e2e.ti.com/support/switches-multiplexers-group/switches…
Part Number: TDA4VH-Q1 Other Parts Discussed in Thread: TS3A27518E-Q1 Tool/software: Debugging Diagnostics Traces
Hello team
I would like to know if the MUX MODE [4] can be changed "on the fly" or Jacinto would need to be flashed
here is the…
Part Number: TS3A27518E-Q1 Hi team,
I have a question about Ik spec definition in absolute maximum ratings section.
Ik is specified as analog port diode current and rated to 50mA with note on (5) as below.
(5) Requires clamp diodes on analog port to V…
Part Number: TS3A27518E-Q1 Other Parts Discussed in Thread: TS3A27518E , SN74CB3T3257 Hi Team,
Whether TS3A27518E-Q1 could achieve logic and also achieve level shift at the same time?
Part Number: TS3A27518E-Q1 Hello Guys,
Good day.
Does the TS3A27518EIPWRQ1 have latch-up protection? Because it was not mentioned on the datasheet. However, the non-automotive grade version TS3A27518EPWR features Latch up protection over 100mA.
Thanks…