Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Hi Louie,
thank you for the measurement. Though, I2C is by far less critical compared to the QSPI use case. The QSPI read speed is 40 Mbps. During QSPI read the TS3A27518E-Q1 switch is two times passed, first the QSPI clock propagating to the QSPI flash…
Part Number: TS3A27518E-Q1 What is the positive supply current for V+ = 3.3V?
Do you recommend placing a cap next to the Vcc pin? If so, what value?
Thanks,
Miles
Part Number: TS3A27518E-Q1 Other Parts Discussed in Thread: TS3A27518E
Hi Team,
We had a question come in that I wanted to double check with you before replying.
Their engineer wants to use the TS3A27518E-Q1 as a 1.8V mux, with VCC at 3.3V. In other…
Part Number: TS3A27518E-Q1TS3A27518E-Q1 will be used in a key position of my customer’s functional safety project. I want to confirm below Items :
what’s the output status when the VCC is under the working threshold, is it high impedance?…
Hello Nitesh,
As the max data rate is directly related to bandwidth, the max frequency data can be passed through the TS3A27518E-Q1 operated at 3.3V at 25C will typically be 240 MHz. However as you suspected, bandwidth varies with Ron and Ron varies with…
Hi,
I would like you to confirm whether following my understanding is correct or not.
Could you please check it ?
* When user set "ENn" pin to "High", then all COMx pins become Hi-z.
(This case is direction of NCx or NOx pins are…
Other Parts Discussed in Thread: TS3A27518E Hi,
I have one question about this device.
* Even though user do NOT supply to V+(Vcc), can user input any voltage (in our case 3.3V) to NCx, NOx and COMx pins ?
Best Regards,
Machida
Part Number: SN74CBTLV3257 Other Parts Discussed in Thread: TS3A27518E , TMUX1574 , TMUX1575 Hello TI experts,
My customer wants to use 1 SPI flash for 2 MCUs, I think they have to use analog SPDT switch for it.
in my searching, SN74CBTLV3257 is suitable…
Part Number: TS3A27518E Hi All,
The customer wants to know the signal trace length limitation of TS3A27518E. Since the DS didn't have a specific constrain for it. Based on your experience, may I know about this part? I also find similar questions but…