Part Number: TS3A5017 We have a question about the TS3A5017 SP4T analog switch.
(1) The following chart’s MOSFET is N type or P type?
(2) See following chart, the “D” means “MOSFET’s Drain terminal” or not
(3) See following…
Part Number: TS3A5017 We built a prototype device that uses 34 of the TS3A5017 IC in the UQFN package. The prototype developed a short between 1S1 (pin 4) and GND (pin 6). We found 3 of theTS3A5017 IC appeared to be burnt on the top of the case above…
Part Number: TS3A5017 Other Parts Discussed in Thread: TMUX136 Hi there,
I want to create a 2:1 switch using an HD-TVI camera ( http://www.ktncusa.com/hd_sdi/hd_sdi_miniature/kez-c2mi4
The control pins have fail-safe logic, the I/O pins have not. There are clamping diodes to V DD , so a current can flow from the I/O pins into the supply.
In general, CMOS switches have low leakage currents, so you should just leave them powered.
There…
Part Number: TS3A5017 Other Parts Discussed in Thread: TS3A5018 Hello sir,
Thanks for your time. I'm wondering what is TS3A5017 RthJC value cause I want to calculate the power consumption and temperature. Could you please kindly provide it to me?…
The TCA9548A-Q1 is the only automotive-qualified I²C switch.
You could use a general-purpose switch like the TS3A5017-Q1, but it would require GPIOs to control it.
Part Number: TS3A5017 Other Parts Discussed in Thread: OPA827 , TS5A3359
Hello Forum,
I try to find a multiplexer for my EMG curcuit. The signal has a bandwith between 10 Hz and 500 Hz and a min Amplitude of 50 uV. I just found one of your analog multiplexers…
Part Number: TS3A5017 My customer is planning to use TS3A5017 . It is expected to pass a 50MHz clock (Square Pulse) which has 0 to 3.3V swing. Any suggestion how good or bad it will be? I see the Frequency/Gain plot in the datasheet and it shows less than…
Part Number: TS3A5017 e2e,
Does TI have a part like TS3A5017 2x 4:1 mux that can handle a 1.8V VIH when VCC is 3.3V? I didn’t see anything on the web. Thanks
Adam