Part Number: TS3A5018 Other Parts Discussed in Thread: TMUX1574 , TMUX1575 Hello, Team
May I know if our TS3A5018 is open-drain design output?
or do we have an device which allow 1.8V supply voltage with open-drain design ?
Part Number: TS3A5018 Hi TI team,
We found that there is something internal pull low when we select the channel.
Please refer the diagram as below, there are 2 cascaded mux switches in the path of our each device.
We set the latter in NO channel.
We…
Part Number: TS3A5018 Hi TI teams.
There is a phenomenon in my case as below. I tried to use the 2 TS3A5018 cascaded in my SPI application.
I'm very confuse about COM3& COM4 delay 452us... and the voltage is rising from 0.8V not 1.8V.
Please refer…
Part Number: TS3A5018 Hi there
Q1. We use two TS3A5018 in series for SPI inerface. I noted in datasheet when the IC is operating at 1.8V supply, the ON-state resistance is relatively lower than 2.5V. (17 ohm VS. 20 ohm). Is that correct or typo?
Q2.…
Part Number: TS3A5018
Hi
Package dimension of those two parts have some difference.
-
-
But both package outline and footprint record on datasheet are the same.
Could you help check if it is correct or not?
Part Number: TS3A5018 Other Parts Discussed in Thread: TMUX1574
Hi
As diagram shows, I use two TS3A5018RSVR series stages for 4 scenario input/output for SPI flash, but I can't get any response, MISO, from my device (SPI flash).
So I want to check…
Part Number: TS3A5018 I'm planning on using this part, but with only two of the four paths. Can I leave the unused pins floating? I'm specifically talking about NC3, NO3, COM3, NC4, NO4, COM4.
Part Number: TS3A5018 Other Parts Discussed in Thread: TS5A2053 , HD3SS3411 , TS3A5223 Hello,
On my PCIE GEN5 Host design I need to support PCIE_REF_CLK (Connector pins A13/A14) to be an input or output from a SoC. The SoC pin is bidirectional.
The clock…