Part Number: TS3A5223 Hi, Ti team
The TS3A5223 has been used in a product with a 5 V system, and the product has already been released to the market.
According to the datasheet, the absolute maximum rating of VCC is 4.3 V, so the device may fail when…
Part Number: TS3A5223 In our application, we are experiencing frequent failures of the TS3A5223. Specifically, there is an internal short (low impedance) between the SEL pin and the Vcc pin within the IC. Even when we try to pull down the SEL pin with…
Part Number: TS3A5223 Tool/software: Dear TI Members
Could you recommend the TI's replacement in stead of ONSEMI's FSA2269?
Size and pin-to-pin compatibility may differ. Please recommend a possible lead package.
(ONSEMI)FSA2269-195533.pdf
Thanks…
Part Number: TS3A5223 Other Parts Discussed in Thread: TXS0102 , LSF0102 , TXU0202 Tool/software: Hi Team,
Customer is planning to use TS3A5223 as a 2CH SPDT MUX for UART.
But since one of the UART is 3.3V, another one is 1.8V, customer is wondering…
Part Number: TS3A5223
Hi,
Customer want to use this switch for headphone analog signal switch between two resources.
If mux switch connect NC1/2 to COM1/2 , is there any DC level still exist on NO1 & 2?
Can these un-used two pin be floating or…
Part Number: TS3A5223 Other Parts Discussed in Thread: TS5A23159 , For TS3A5223 (and TS5A23159), what happens in NC/NO/COM have voltages applied before VCC is present? I understand this can cause the internal ESD diodes to conduct but what is the consequence…
Hi Scott,
Thanks for posting, welcome to E2E!
Is this the reference design you are wondering about? These devices are simply suggestions and can be used as a starting point for your design. You will need to make sure that any switch/multiplexer you…
Part Number: TS3A5223 Hello,
I had a customer ask if there was an IBIS model available for the TS3A5223. I'm not too familiar with what this is. Could you please explain and provide if it is available to share with the customer?
Thank you,
Kyle
Part Number: TS3A5223 Hello,
I'm looking for P2P replacement for ET5223. Link is below.
http://www.etek.com.cn/en/product.asp?id=332
file:///C:/Users/a0486368/Downloads/datasheet.pdf
Looks TS3A5223 can be directly replaceable P2P device but…