Part Number: TS3DDR3812 Other Parts Discussed in Thread: TS3DDR4000 , TS3DV642 , Hi Team,
I want to know the current consumption of TS3DDR3812 .
I can find ICC is averagely 300uA on VCC = 3.6 V, II/O = 0, VIN = VDD or GND.
My customer will use TS3DDR3812…
Part Number: TS3DDR3812 Dear experts,
I need a switch SPDT that can pass both differential and single ended signals.
I am muxing RGMII signals with 1000b Ethernet signals for use with a two different SOM's, system on module.
I have 12 signals that…
Part Number: TS3DDR3812 I would like to obtain an S-parameter model for this part number for internal simulations, if it is available. In lieu of that, a simple lumped RLC model would also work.
regards,
-Shriram
Part Number: TS3DDR3812 Hello,
Ours customer bought TS3DDR3812RUAR from TI estore, and found that the appearance is abnormal, the die attach is not flat, please refer to the below picture: the arrow of the red mark is abnormal. The order number is T00953032…
Part Number: TS3DDR3812 Poor quality Number: CS0273767 Contact: SANDY CHIANG
Product name TS3DDR3812RUAR~TI Bad number: 1
Currently only use 557PCS to check all Found 1PCS abnormal Cause of abnormality: The gold wire is twisted and the function is…
Thank you for the response.
Can I assume that the max value for the switching time would be 7ns from the moment we toggle the Select line?
Parker Dodson said: For the TS3DDR3812 tPZH and tPZL represent "Enable Time" from the select input. This along…
Part Number: TS3DDR3812 My customer needs to isolate RGMII signals when some circuit (CPU) is not powered up. They are using TS3DDR3812RUAR as an isolation barrier.
Will TS3DDR3812RUAR carry the RGMII signals without introducing any issues?
are…
Alexey,
I apologize for the delay but I could not locate hardware in the lab to be able to make this kind of measurement. We would have to create hardware to make this measurement.
Adam