Part Number: TS3DV642-Q1 Other Parts Discussed in Thread: TS3DV642 Hi,
We are using CEC and HPD as differential pair. CEC connected to P channel and HPD connected to N channel whether we can swap P and N differential pair or any default P and N configuration…
Part Number: TS3DV642-Q1 Other Parts Discussed in Thread: TS3DV642 , hi team,
i have two question about the device,
first what the difference of TS3DV642RUARQ1 with TS3D642A0RUAR. i see the datasheet TS3DV642-Q1 can support MIPI, but the datasheet of TS3DV642…
Part Number: TS3DV642-Q1 Hi Experts,
Good day.
About TS3DV642-Q1, we wanted to know whether we can switch the input side differential pair (as in can we connect DP from the host processor to DN in the mipi switch and DN from the host processor to DP in…
Part Number: TS3DV642-Q1
Above is TS3DV642-Q1 demo design.For part A, why does HDMI and I2C connect to VCC with 0Ω resistor? Is it for sink termination ? and there is no mention the level of VCC .
Below is our use case, Whether partA is required or the…
Part Number: TS3DV642-Q1 Hello,
is there any further information about the propagation delay of the device. Is there a maximum value?
Our idea is to use two of these devices to switch the input from two deserializer (A and B) with odd and even pixel lanes…
Part Number: TS3DV642-Q1 Hello,
is there any further information about the propagation delay of the device. Is there a maximum value?
Our idea is to use two of these devices to switch the input from two deserializer (A and B) with odd and even pixel lanes…
Part Number: TS3DV642-Q1 HI EXPERTS ,
I HAVE DESIGN THAT I USE THIS MUX AS MIPI MUX.
1. AT THE EVB OF TI RELATED TO THIS MUX ALL THE DATA LANES ARE CONNECTED TO 0.22U CAPACITOR DOES IT NECESARY?
2. AT THE EVB, THE MUX OUTPUT LANES ARE CONNECTED WITH 0…
Part Number: TS3DV642-Q1
Hi Team,
Good day.
Our customer is asking if we now have an available S-parameter for TS3DV642-Q1.
Thank you.
Kind regards,
Marvin