Part Number: TS3V712EL Hi team,
Could you please share what's the difference between these two devices, from performance and HW design point of view? Thank you.
TI PN: TS3V712ELRTGR
5-V, 1:2 (SPDT), 7-channel VGA SPDT switch with level shifters…
Hello expert,
Customer's MB already transfer HSYNC/VSYNC/DDC/DAT to 5V level ,the TS3V712E have no level shift function.
The TS3V712E spec VDD is 3.6V max and VI/O is 0~VDD ,so we must use TS3V712EL or TS3V713EL. Is that correct? Thanks a lot!!
Best…
Hi Simon,
It should be the same (1 uA).
Ioff is the maximum leakage current into an input or output terminal of the device, with the specified voltage applied to the terminal and VCC = 0 V
The Ioff protection circuitry ensures that no excessive current…
Hi Tom,
Thanks for the information!
So first off - this switch cannot pass negative signals - so if the 1Vp-p is centered at 0V there could be issues passing the signal without issue either with quality of signal or damage to the switch as it has a…
Frank,
You can use the TS3V712EL datasheet typical circuit for guidance. The main difference between the TS3V712E and the TS3V712EL is the additional features of integrated level shifters on the Hsync and Vsync pins of the TS3V12EL IC.
Typical application…
Other Parts Discussed in Thread: TS3V712EL , TS3V712E , TS3V713EL Hi team,
My customer is looking for KVM solution. For two VGA in, one VGA output, we find the TS3V712E(we think the TS3V712EL cannot be used here, the TS3V712EL maybe only can be used for…
Part Number: SN74CBT3251 Other Parts Discussed in Thread: SN74CBT162292 , SN74CBT16292 , SN74CBT16232 , SN74CBT16390 , SN74CBT3257C , SN74CBT3257 , TS3V712EL , TS3V713EL , TS5V330 , TS5V330C Hi Sir
May we know if SN74CBT3390 already obsolete?because i can't find…
Part Number: TS3V713EL Other Parts Discussed in Thread: TS3V330 , TS3V340 , TS3V712E , TS3V712EL I need to take 10 VGA sources (ports) and multiplex down to 1 output monitor display.
The TS3V713EL says it can be used as a 2:1 mux. Do I take 9 of these devices…
Other Parts Discussed in Thread: TS3V712EL , TS3DV642 Hello Team,
I'm looking forward to the HDMI/LAN/VGA/DDR/Video Switch which has strong CDM (higher than 1kV).
However some devices don’t have CDM rating in its datasheet. (e.g. TS3V712EL etc..)…
Other Parts Discussed in Thread: TS3V712EL , TS3V712E Hi,
As far as I search, there is no IBIS model for both TS3V712E and TS3V712EL.
Do you have any plan to create it?
If you already have it, can you please share with me?
Thank you for your support in…