Other Parts Discussed in Thread: TS3V713EL , TS3V712E hi all,
I want to make vga switch used ts3v713el(2 in 1 out),but this is a promblem now.when the chip is powerdown,the input hsync&vsync signal voltage level is normal (5V,negative pulse).if the chip…
Johnny,
I pulled the PI3V713-A datasheet from pericom's website and see that for the PI3V713-A device you are correct you need to pull up pin 8 Reserved pin "high".
Since the TS3V713EL does not have a bond wire connecting pin 8 to the…
Part Number: LMH6572 Other Parts Discussed in Thread: OPA3875 , TS3V713EL Hi Experts
We are finding VGA RGB signal 4(input) to 1(output) mux for the server product ,I see the LMH6572 may meet this application.
1. Please double check the application
2. Please…
Mike,
The TS3V713EL integrated level shifters are unidirectional. This means the Hsync/Vsync signal paths are not bidirectional in the TS3V713EL.
If you would like a similar device that is bidirectional on all signal paths I would look at using the…
Chasel,
The relationship between bandwidth and resolution calculation requires more variables than you specified.
For more details you can see this application note Signal Bandwidth vs. Resolution for analog Video.pdf
A very conservative and simplified…
Part Number: TS3V712E Other Parts Discussed in Thread: , TS3V713EL Hello expert,
May we know the difference between TS3V712E/712EL/713EL? Thanks!
Best regards,
Ann Lien
Hi Tom,
Thanks for the information!
So first off - this switch cannot pass negative signals - so if the 1Vp-p is centered at 0V there could be issues passing the signal without issue either with quality of signal or damage to the switch as it has a…
Part Number: TS5V522C Other Parts Discussed in Thread: TS3V713EL Dear Sirs,
The datasheet mentioned that can be to do bus Isolation.
My I know it can be to do VGA signals isolation?
Hi Sanjay,
Unfortunately, we do not have a Q1-Grade mulitplexiers that can meet 300MHz video requirement. Is the customer pusuing the device or are they considering using 2:1 video mux for future design.
In terms of 2:1 video mux, we actually have…
Part Number: SN74CBT3251 Other Parts Discussed in Thread: SN74CBT162292 , SN74CBT16292 , SN74CBT16232 , SN74CBT16390 , SN74CBT3257C , SN74CBT3257 , TS3V712EL , TS3V713EL , TS5V330 , TS5V330C Hi Sir
May we know if SN74CBT3390 already obsolete?because i can't find…