Part Number: TS5A2066 Can the following TI parts go thru a PCBA wash process using deionized water or kyzen A4625B? See attached list.
Wash_TI_Parts.xlsx
Part Number: TS5A2066 Tool/software: Hi TI team,
I have enquiries about appearance specification for below MPN.
For info, this component was found chip-off but after investigation the cause of this chip-off is due to our nozzle pickup and placed…
Part Number: TS5A2066 Other Parts Discussed in Thread: TS5A23166 , TS5A21366 Hello,
Does this device have positive clamping diodes on VIN?
Basically, trying to understand if I can apply 5V to VIN or NO when VCC is 3.3V. I read the footnote that "The…
Part Number: TS5A2066 Other Parts Discussed in Thread: TS5A21366 , TS5A23166 Hello,
I am using the TS5A2066 in my design, but I need high impedance on its outputs when there is no Vcc (device OFF). This device partially provides the input voltage when…
Part Number: TS5A2066 On page one of the datasheet (looks like Rev F) it shows the part dimensions for the DSBGA package as 1.25 mm x 2.25 mm
In the package description on page 34 it shows the dimensions as 1.9 mm x 0.9 mm
Which one is correct…
Part Number: TS5A2066 Let me know if the six products are EAR99 or not.
1_TS5A2066YZPR
2_TPS65261-1RHBT
3_TLV75509PDRVR
4_TLV71725PDQNR
5_TLV71718PDQNR
6_LP5907SNX-2.9/NOPB
Thanks.
Hi Adam,
Thank you for the help!
I'm actually working on a list of the best TI crosses to leverage against competitor parts, so I am more trying to find a part that best fits as a replacement to the comp part rather than satisfy a specific requirement…
Part Number: TS5A2066 E2E,
I use TS5A2066, but it’s VDD is 5V and control signal is 3.3V for logic high. As the datasheet shows, when VDD is 5V, the digital control signal need to be higher than 5V*0.7=3.5V.
So my question is if I continue to use…