Part Number: TS5A21366 Other Parts Discussed in Thread: TMUX1511 Hi :
In data sheet, it said that the firee-air temperature of TS5A21366 is -40--85C.
My question is what will happen if I use TS5A21366 in 100C?
Our product need to survive in 85C…
Part Number: TS5A21366 Other Parts Discussed in Thread: TS5A23166 Hi Team,
Please see below measurement. We found that TS5A21366 has some undershoot but TPS5A23166 is ok when Switch OFF (IN=L) .
Below is the measurement of TS5A21366. And TS5A23166…
Part Number: TS5A21366 If Vcc = 0V, will the IC fail if an analog voltage is input under the following conditions?
【conditions】
Vcc = 0 [V]
NO1 = 5 [V]
NO1(max current) = 1 [mA]
time = 1ms
Part Number: TS5A21366 Other Parts Discussed in Thread: TCA9800 , TCA9406 , TXS0102 Hi Sirs,
Sorry to bother you.
We would like to use TS5A21366 on I2C
If the COM side have PU to 1.8v, NO side have PU to 3.3v. VCC is 3.3v.
Have any risk on our…
Part Number: TS5A21366 Hi Team,
Can IN1/2 = 3.3V when use 1.8V at Vcc?
Based on spec, the maximum input voltage is Vcc. It seems like this violate spec.
Shaq
Part Number: TS5A21366 Other Parts Discussed in Thread: TS3USB31E Hi team,
My customer wants to use one switch to block/bypass differential signal.
They're wondering whether the 2CH SPST switch TS5A21366 could act as a differential signal switch.…
Part Number: TS5A21366
Hi experts,
Can TS5A21366 switch negative voltages (-200mV to GND) at the NOn and COMn pins? Any concerns?
Thanks and BR, KF.
TS5A21366DCUR
Part Number: TS5A21366 Other Parts Discussed in Thread: TS5A23166 , TS5A23157 My customer uses MAX4619 as a signal isolator and 2:1 MUX. They like it because it has -93dB off-isolation and -96dB crosstalk. The signal they are trying to isolate and pass…
Part Number: TS5A21366 Other Parts Discussed in Thread: TS5A3166 I was looking at the datasheet of TS5A21366 and there is a mention of connecting the ground to a digital ground. Why can't it be connected to an analog ground? What is the reasoning behind…
Part Number: TS5A21366 Other Parts Discussed in Thread: TS3USB31E , TS5A9411 , SN74CBT3306 , TS5A623157 , SN74CBT3305C , TS5A63157 Hi,
I need an analog switch with very low OFF capacitance on its output (capacitance during off state).
At the moment…