Part Number: TS5A22366 Dear Specialists,
My customer is considering TS5A22366 and has a question.
I would be grateful if you could advise.
---
On pages 25-26 of the datasheet, there is a description "SOLDER PASTE EXAMPLE".
In this case, what…
Part Number: TS5A22366 We are looking at the bottomside of TI BGA part TS5A22366 image. Seems like it is just a bare silicon. We are wondering if there is any insulation layer, to protect the silicon from shorting to the solder ball, during reflow. I…
Part Number: TS5A22366 Hi Team,
The THD test circuit is as below. May I know:
1. Will the THD be better if the CL is less than 50pF?
2. What are the limitations for MUX THD?
3. Is there any other dual SPDT with higher THD such as 110dB? Because the MUX is…
Thai,
TI has over 300 switches to choose from that will support wide range in voltages. Ti.com switch search tool will allow you to use the power supply filter Vcc max to find a device that will support the voltage you need. Below I filtered for 2:1,…
Part Number: TS5A22366 Other Parts Discussed in Thread: TS5A22362 , TS5A22364 Hi,
with reference to the application block diagram of TS5A22366, i needed some verification on the status of switch position when there's no inbound Vcc into the device. With…
Part Number: TS5A22366 Hi,
I understand that NC pin has no internal connection, so it can be tied to GND. Is my understanding correct?
Best Regards,
Satoshi / Japan Disty
The speed of I²C rising edges is limited by the low-pass RC filter formed by the pull-up resistors (in this case, two in parallel) and the total bus capacitance. The TS5A22362 has a specified capacitance of 370 pF, which is near the upper I²C limit of…
Ranita,
The TS5A22366 2-channel 2:1 audio switch is a great choice to replace the NLAS2750 2-channel 2:1 audio switch. The biggest difference between the two is the NLAS2750 comes in a QFN package but the TS5A2366 comes is a smaller BGA package.
TI also…
Other Parts Discussed in Thread: TS5A22366 Hi,
I downloaded the .bxl of the TS5A22366 and I am a bit confused!
On the datasheet the YFC PACKAGE TERMINAL ASSIGNMENTS is
However, when I verify in Eagle the pin out is different
Could you please confirm me…
Other Parts Discussed in Thread: TS5A22366 , TS3DS10224 Team,
My customer is looking for a bidirectional 1:4 mux/demux.
I’m noticing we only have dual 1:4 devices, they want a single that can do 1:4 and handle bidirectional signals.
I’m thinking they…