Part Number: TS3A5223 Other Parts Discussed in Thread: TS5A22362 , TS5A22364 , TS5A22366
Hi Expert,
If TS5A223 Vcc=0, SELx=0, does NC1=COM1 and NC2=COM2? Or other analog switch can support it. (headphone signal.) Thanks!
Martyn,
Do you have scope captures of the waveforms passing through the switch when the switch is on and off? COM, NC, and NO ?
The TS5A23159 device is not specified to pass signals < 0 V.
If you would like and audio switch that can support negative…
Other Parts Discussed in Thread: TS5A23159 , SN74LV4053A , TS5A22366 , TS5A26542 customer is asking for an alternative to ADG1633BCPZ-REEL7 from ADI. Is TS5A23159 our best alternative? do we have anything better?
OD,
If your signal is going to centered at 0 volts you will need to select a switch that can support a negative signal. You can find these devices with the TI.com switch selector tool.
Here I filtered on 2-channel, 2:1, and can have the I/O signal <0…
Tao_2199
1) You are correct, power consumption information (operating supply current) comes from page 7 and 8 in the datasheet. Typically you can expect 0.2 uA with Vcc = 5.5 V, Vcom = Vcc or GND, and Vin = Vcc or GND. Also remember the statement in note 2 below…
I haven't seen such an implementation before, but the TS5A22366 is a 1:2 mux that may be suitable for switching between the D inputs and R outputs of two RS-485 transceivers.
Kensuke,
I have looked through my products and could not find something that met all of your requirements.
I listed some switches that are negative signal capable: TS3USB225, TS5A22362, TS5A22364, TS5A22366.
I have copied an application engineer that…
Hi Jason,
TS5A22366 can support -3/5.5V voltage range and TS12A12511 can support 2.7V-12V range voltage supply.
We don't have switch which support +/-12 V input.
I think some amplifier can meet your requirment (+/- 12 V in, 0/5V output).
Tha…
Michael,
The TS3A44159 is not capable of passing an audio signal because as you mentioned the "Analog voltage range -0.5V ... V+ + 0.5 V" does not support a negative swing. We do have several general purpose switches that can support signals with negative…
Other Parts Discussed in Thread: TS12A44513 , TS3A227E , TS12A4517 , TS5A22362 , TS12A4516 , TS12A12511 , TS5A22364 , TS5A22366 Hello, all
Now we have one inquiry regarding suit solution for bipolar input capability on analog switches from our customer.
Please…