Other Parts Discussed in Thread: TS5A23157 Hi ,
could TI provide complete TS5A23157 Pspice model (*.dsn) ?
I transfer TS5A23157 ibs model ,
I found it just have input pin only (from transfer TS5A23157 ibs model ) ,
no any library have complete module with all…
Part Number: TS5A23157 Hello,
My customer considers using the TS5A23157 for the following application.
- Connect BLE UART and AP UART to RS232 Transceiver
- UART_MUX_DIR is controlled by AP and in default state, they want BLE UART and RS232 Transceiver…
Part Number: TS5A23157-Q1 Other Parts Discussed in Thread: TS5A23157 Hi Team,
Recently, during customer's PV experiment, customer found that the TS5A23157DGSRA package bulged and failed as following picture.
What kind of problems or conditions will…
Part Number: TS5A23157-Q1 Hello team,
My customer has related questions about TS5A23157-Q1 as below, could you please give a detailed explain about each condition.
(1) If the V + power supply is 3.3V and the input and output signal (no, NC, COM) level…
Part Number: TS5A23157 Other Parts Discussed in Thread: TS5USBC41 Hi,
For KTU1188G, does TI have replace solution?
KTU1188G-03a_dms03.pdf
Is TS5A23157 suitable?
Thanks!
Jeff
Part Number: TS5A23157-Q1 Hi team,
My customer are looking for a socket used for switching two channel TDM signal to one channel TDM signal? Do we have related socket recommend? Thanks!
BR
Jiawei
Part Number: TS5A23157-Q1 Hi TI:
We found the VIH-min is V+*0.7(2.31V) for 3.3V supply.
In fact we used 1.8V in IN1 pin,that can also to select NO to COM.
Can we use 1.8V in IN1 pin to select channel in 3.3V system?
What is the risk of it ?
Thanks!!
Part Number: TS5A2053 Other Parts Discussed in Thread: TS5A23157 , , TS5A623157 , TMUX1072
Hello there,
As I found a lot of inventory of TS5A2053 in ti.com, I'm thinking to suggest my customer to replace TS5A23157 with TS5A2053. The application is protection…
Part Number: TS5A23157 Other Parts Discussed in Thread: TS5A23159 Hi team,
could you help confirm the normal current capacity of the lower gate voltage switch TS5A23157? For example, the output voltage will not change if the normal 30mA current flows…