Part Number: TS5A23157-Q1 Hi team,
My customer are looking for a socket used for switching two channel TDM signal to one channel TDM signal? Do we have related socket recommend? Thanks!
BR
Jiawei
Part Number: TS5A23157-Q1 Hi TI:
We found the VIH-min is V+*0.7(2.31V) for 3.3V supply.
In fact we used 1.8V in IN1 pin,that can also to select NO to COM.
Can we use 1.8V in IN1 pin to select channel in 3.3V system?
What is the risk of it ?
Thanks!!
Part Number: TS5A23157-Q1 Hi Team,
We occur the issue using TS5A23157-Q1. Below is our connection. We used TS5A23157-Q1 to switch the I2C signal. (400kHz)
Below is the config.
SW = 1
CH1: U801_SDA, CH2: U801_SCL, CH3: U802_SDA, CH4: U802_SCL …
Part Number: TS5A23157-Q1 Hi sir,
My customer need TS5A23157QDGSRQ1 Tjc thermal impedance information. Can you please provide this data? if no data on hand, when can you please give the data? Thanks.
Part Number: TS5A23157-Q1 Hi TI expert
I looked the datasheet and it was unmarked ADAS information,please tell me whether TS5A23157TDGSRQ1 can be used in ADAS application and ADAS products (QM/A/B/C/D) is QM?
Thanks
Jacob
Part Number: TMUX4052-Q1 Other Parts Discussed in Thread: TMUX1309-Q1 , TS5A23157-Q1 , SN74LVC2G17 , SN74LVC1G08 , TS3USB221A-Q1 Find a URAT MUX,One Chanel URAT is converted to two outputs, 2chanel,2:1MUX,automotive application
Part Number: TS3USB221A-Q1 Other Parts Discussed in Thread: TS3USB221 , TS5A23157-Q1
Hi, Support Team
Can TS3USB221 be adopted for UART interface?
I/O voltage: 1.8V
for passive switch,
if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrenc…
Part Number: SN3257-Q1 Other Parts Discussed in Thread: TMUX154E , TMUX136 , TS5A23157-Q1 Hi TI Expert,
May I know whether SN3257-Q1 can support I3C function?
The spec of it should be able to cover it, same as TMUX154E & TMUX136.
Kindly let us know…
Hi Sam Lee,
The power consumption for the TS5A23157-Q1 across full temperature range –40°C to 125°C is <10uA. You can see in the I+ spec in the datasheet.
Thanks
Saminah
Other Parts Discussed in Thread: TS5A23157-Q1 , TMUX136 , TS3DV642-Q1 Hi team,
Do we have any device that can support 2 to 1 mux for LVDS signal? My customer has such demand in Auto IVI application. They need to transfer a video signal with 1920*720@60Hz…