Part Number: TS5A23159 I have seen in the datasheet that the maximum ambient temperature in operation is 85°C and that the maximum storage temperature is 150°C. But I would need to know the maximum juntion temperature to estimate if the measured casing…
CCI is a subset of I²C. The TCA9543A works on the electrical level, so it supports CCI.
(The TCA9543A is controlled through the same I²C bus. A general-purpose analog switch like the TS5A23157 or TS5A23159 would be cheaper, but would require a separate…
Part Number: TS5A23159 Other Parts Discussed in Thread: TS5A22364 : I am trying to switch 8 ohm speakers. When switched off there still is a scratchy sound coming though from the amplifier. The speakers are not completely switched off. I have tried a…
Part Number: TS5A23159 Other Parts Discussed in Thread: ADC121S101 , SN74LV4051A , Hi
We are using analog mux SN74LV4051A with ADC121S101.
8x Inputs -> SN74LV4051A -> ADC121S101
This time, we are considering 2:1 mux (or switch) and we are going to…
Hi again,
I finally found what was causing the issue. I understood after I had a look with an oscilloscope, here is the MISO/POCI (line 1) with the Clock (line 2). Clearly something was preventing the PGA from pulling the line to a low level, and that…
Part Number: TS5A23159 I used the TI cross-reference tool to find a part to replace the ADG736. The cross-reference gave me the TS5A23159 and stated that this was a direct replacement (code S). Looking at the datasheets, the TI part and the Analog Devices…
Part Number: TS5A23159 I am using a TS5A23159 Analog Switch and the switch on-voltage at ~ 10uA current is 0.4 volts. Is this expected behavior? Can anything be done to get low on-state voltage under these conditions? The part also seems to be drawing…
Hello, Adam.
I want to know whether TS5A23159 can be applied the case that the switch frequency is 5MHz ?
I found the output of the chip appeared signal distortion under such high switch speed.
The yellow waveform is the IN1 (Pin 1), the blue waveform is…
Part Number: TS5A23159 Other Parts Discussed in Thread: TS3USB221 Hello, I am having an issue with a TS5A23159RSER SPDT switch deployed in a product. We are using the switch to pass either USB D+/D- or 3.3v UART Rx/Tx signals to a micro-b USB connector…
Gianluca,
The TS5A23159 will be able to pass a 13.36 MHz signal without issue as long as it is within the recommended operating conditions stated in the datasheet.
The most common issue that comes up with the term "RF" signal is people are reffering to…