Part Number: TS5A26542
I have a customer asking about the current consumption under the following conditions. If possible, I need to provide an estimated max current consumption during such a use-case.
V+ = 5.1V Vio = 1.8V IN1, IN2 = MAX 2.3V NOx…
Hi Ian Wang,
we don't put in this feature in our devices compared to power switches. How ever, depending on your exact need, we could find a switch with adequate ton.
Can you tell us your required configuration?
Best regards,
Ambroise
Part Number: TS5A26542 Max switching current for this device given as 700mA and continuous 450mA. Are there any other bidirectional devices with similar or higher max current. Device can be N/O. ? Is there a device with this current capability in a different…
Part Number: TS5A26542 Other Parts Discussed in Thread: ADS114S08 , TMUX1119 , TMUX1108 , TMUX1109 Hello,
I am designing an instrumentation circuit with ADS114s08, and I am planning to use TS5A26542 switch for the following purposes:
1. Routing thermocouple…
Hi Adam,
THe TS5A26542 has a seperate VIO rail in order to minimize power consumption when operating at a high supply rail (3V or 5V) but only a 1.8V logic signal.
Please see the below image which lists the range for VIO to 1.65V to 1.95V and the…
Part Number: TS5A26542 Other Parts Discussed in Thread: TMUX136 Dear Team,
TS5A26542 has a great feature of Input Logic Translation. The Vio range is only specified from 1.65 to 1.95V - Is this range extendable?
Thanks and regards
Part Number: TS5A26542 Hello
can the switch I\O operate at Vio=+5V , IN1,IN2 = Vio levels (0 & +5 V)
consider the max Vio should be less than 6.5V ,it shouldn't be a problem .
i would like to validate that
thanks
Gil Rafalovich
Other Parts Discussed in Thread: TS5A26542 Hello,
I looked at the datasheet and I haven’t found any information regarding the max junction temperature of the part TS5A26542. I have only found the maximum package thermal impedance , but I am not sure…
Other Parts Discussed in Thread: TS5A26542 TI Team,
I would like to get some clarification about the TS5A26542 SPDT analog multiplexer. The datasheet is not clear about the conditions under which a switch pin is left unconnected. Here are my queestions…
Part Number: TLV320AIC3100 Other Parts Discussed in Thread: TS3A24157 , TS5A26542 Tool/software: Hi Gilgur-san,
Thank you reply.
My request is to find lowest device that meets following specifications:
"2:1 2-channel device" used to switch…