Part Number: SN74LVC1G3157 Other Parts Discussed in Thread: TS5A3159-EP We are looking to secure this exact same part (SN74LVC1G3157) but with a -55C to +70C operating temp. Is that something that is available?
Zhengqing,
TI uses suffix letters to mean several different things depending on the device so it is good to ask what it means. For this example the TS5A3159a is a new device revision that added a new BGA package and new powered off protection feature…
Part Number: TS5A3159 Hi,
When add a 10K pull-down resistor at pin IN, the voltage of IN is only 1.0V even the Pull-high voltage is 3.3V. Change 10K to 100K, result is the same, but voltage getting 3.3V after remove pull-down resistor.
1. What is the input…
Bo345,
I used the ti.com switch search tool to find a 1-channel, 2:1 switch, in a SOT-23 package. The results that came back meet all your requirements except same pinout. I filtered on the criteria and then sorted on price. I would suggest using the low…
Part Number: TS5A3159-Q1 Other Parts Discussed in Thread: TS3A27518E-Q1 Does anyone have an idea of what the propagation time of this switch is under these conditions:
1) the 'IN' pin (pin 6) is static at say logic high (This is the switch control pin…
Part Number: TS5A3159 Other Parts Discussed in Thread: TMUX6104 Hello,
I have a question about TS5A3159 analog switch. What a voltage level allowable between NC pin and ground when NC pin is in OFF state? 24 V allowable or not?
Thank you.
Part Number: TS5A3159 Dear team,
Could you please explain more details about TS5A3159's leakage current specification like INC(off), INC(on) and ICOM(on)? How do we measure these parameters and what is current flow direction of INC(off), INC(on) an…
Part Number: TS5A3159-Q1 Other Parts Discussed in Thread: TAS5411-Q1 e2e,
Will the TS5A3159-Q1 have the ability to switch between one speaker or another in the use case below?
Thank you,
Adam
Part Number: TS5A3159 Other Parts Discussed in Thread: , SN74AUC2G53 Hi Team,
I would like to know will COM pin short to NC pin when TS5A3159 has no any power supply on V+?
What is the status of the internal switch?
Thanks.