Part Number: TS5A3159A Hi Team,
Working on the TS5A3159A. We did an isolated test on TS5A3159A since it is used in many designs and it keeps coming back with the following issues:
Select input is digital 5v tolerant: it can go above VCC up to 5v, but…
Part Number: TS5A3159A Hello, Could you provide max. operating junction temperature for this device? I only see max operating ambient rating and would like to see junction rating
Best regards,
Part Number: TS5A3160 Other Parts Discussed in Thread: TS5A3159A , TS5A3159 HI,
Could you please let me know the differences between TS5A3159 and TS5A3159A?
I found Ron of TS5A3159 is smaller than TS5A3159.
- Is the material of bonding wire same? - Are there…
Part Number: TS5A3159A Other Parts Discussed in Thread: TMUX1072 , TS5A9411 , TMUX154E , TMUX1136 , TMUX1575 , SN3257-Q1 Team,
We use TS5A3159A to achieve video signal switch. The frequency is 41MHz and 36MHz. Could you help find the better crosstalk part…
Part Number: TS5A3159A Other Parts Discussed in Thread: TS5A3159 , , TMUX1102 , SN74LVC1T45
I am using the TS5A3159 as a switch to test battery voltage and found that the device is drawing excessive current. Please see the attached schematic showing the…
Part Number: TS5A3159A HI TI team:
Can you help provide below information
Description
供应商
Factory Name(工厂名字)
Factory Address Line 1(工厂地址)
Factory City(工厂城市)
Factory State/Province(工厂省份)
Factory Postcode/Zipcode(工厂邮编)
Factory Country…
Part Number: TS5A3159A Hello,
Om page 6 of the datasheet, maximum INC(ON) and INO(ON) over full temperature are specified 20nA at V+=3.3V.
However, looking at figure#5 on page 11, they are around 30nA at V+=3.6V, it exceeds the maximum spec on page 6…
Part Number: TS5A3159A Hi Sir,
My customer is using TS5A3159AYZPR on their system and facing a cross talk issue.
Could you help to advise if we have a P2P solution with higher cross talk isolation spec?
The signal is a video data and data rate as below…