Part Number: TS5A3166-Q1 Hi Experts
I am trying to verify the Input leakage current spec in the datasheet.
I am applying 5.5V to the V+ supply pin and then sending +5.5V and/or 0V to IN (pin 4).
I see leakage of 89nA at V_IN = 5.5V, and 123nA with…
Part Number: TS5A3166 Dear Team,
I am using TS5A3166 in one of my applications.
Whenever I want to enable it ,I am planning to connect it to Vcc using a Jumper.
My circuit is given below.May I know it is fine or not.
Regards
HARI
Part Number: TS5A3166 Other Parts Discussed in Thread: SN74LVC2G66 , What's the difference between TS5A3166 and SN74LVC2G66>
Is TS5A3166 bidirectional ?
Regards
Brian W
Part Number: TS5A3166 Hello Team,
can you provide typical figure about noise spectrum density of analog switches (e.g. TS5A3166 would be of interest), please?
Especially flicker noise would be of interest.
Thanks and Best Regards,
Hans
Part Number: TS5A3166 Other Parts Discussed in Thread: SN74LVC1G3157 Mux Experts,
The power off behavior of this device is causing me considerable consternation.
In the parametric search this device is listed as having power off protection.
The…
Hi Kaveh,
Thank you for pointing this out. The TS5A3166-Q1 datasheet pin NO is normally open. This a mistake on the datasheet and we will update the correct pin description.
The testing and qualification required for them are different. The TS5A3166…
Part Number: TS5A3166 Other Parts Discussed in Thread: TS5A22364 Hi team,
Do we have any SPST switch and SPDT switch for audio application?
Thanks and Best Regards,
Will
Part Number: TS5A3166 Good day,
One of my customer plans to use TS5A3166 and there is a question about possible operation mode. Can this device held impulse with following parameters or it will be damaged: amplitude from -0.6V to -9V (negative voltage…
Part Number: TS5A3166
Are the TS5A3166 5v operation switch specifications guaranteed with the IN control voltage between 0v and 0.8v for OFF, and between 2.4v and 5v for ON? Is a SPICE model available?
Part Number: TS5A3166 Other Parts Discussed in Thread: TS3A24159 Dear team,
My customer consider using TS5A3166 for Current Transformer application.but there is issue on that.
- Vcc : 3.3V
- IN signal : high , Rds on 0.9~1.1 ohm It is OK. but IN…