Part Number: TS5A3166-Q1 Other Parts Discussed in Thread: THVD1419 , SN74CB3Q3306A , SN3257-Q1 Hi All,
I'm planning to design a system with RS485 transceiver (THVD1419), and want feature of turning ON/OFF the termination through micro-controller.…
Hey D, I'm not quite sure where you're seeing the YPZ package. Perhaps you've inadvertently looked at the catalog TS5A3166 datasheet instead of the automotive TS5A3166-Q1? Here's what I see on the datasheet for packages on the Q1 version. So there's only…
Part Number: TS5A3166 Hi,
I have two questions regarding TS5A3166:
1. Is there a difference between the currents of the NO and COM pins?
For instance if a 5mA current is driven from the NO pin, what is the expected current at the COM pin (and…
Part Number: TS5A3166 Hello Team, Good day. Our customer intends to use the TS5A3166 as a low-side switch for 4 load cells. They intend to add the switch into the ground to switch all 4 load cells at once, then read the signals separately through an ADC…
Sebastien,
The TS5A3167 and TS5A3166 devices should have they same bandwidth since the only difference between them is the logic control.
It looks like in 2005 the datasheet had the bandwidth for both devices at 200MHz for all supply voltages. In…
Part Number: TS5A3166 Will COM be shorted to GND when V+ is still unstable during power-on?
Will COM connect with NO when V+ is still unstable during power-on?
What state is COM when V+ is still unstable during power-on?
Part Number: TS5A3166-Q1 Hi Team,
There is a confusing explanation about the ONOFF logic in its datasheet, so please check it just in case.
Is "NO to COM" path shorted when high logic is applied to IN pin? Or Open?
I can find following table on…
Part Number: TS5A3166 Other Parts Discussed in Thread: TMUX1101 Hi , I can see this part in SOT23 flagged as "Available until stock is exhausted" in Farnell.
Could you confirm if there are plans to obsolete the SOT23 version ie TS5A3166DBVR in near…
Hello Adam !!
sorry finally we have understand that the component is working very well !
It was an our measuring problem.
Thank you for your support .
Alice Paolo
HEIDENHAIN ITALIANA S.r.l.