Part Number: TS5A3167 Other Parts Discussed in Thread: TS5A3166 , , TS5A4594 Tool/software: The banner title of the datasheet says this is a SPST BUT the Description says its a SPDT (DOUBLE throw, rather than SINGLE throw. The rest of the datasheet docuements…
Part Number: TS5A3167 Tool/software: Hello TS5A3167 supports isolation in powered-OFF mode and it is defined like the below which is marked as yellow.
Is this leakage curret flow from "NC or COM" to GND(or VCC?)? or "NC or COM" to "COM or NC"? If…
Part Number: TS5A3167 Hello TI support,
We intend to use TS5A3167 to switch 2.5V supply to peripherals on other side in battery application. We need information on Inc/ Icom (OFF) leakage current when Vnc/ Vcom are from 0 to 2.5V for VCC=2.5V condition…
Part Number: TS5A3167 Hi there,
Could you inform me about the terminal finish of the part TS5A3167DBVR. Could you tell me the thickness of Au in case the terminal finish is NiPdAu or NiAu or Au.
Thanks.
Best Regards,
Kaoutar Ben Kaddour
Part Number: TS5A3167 Other Parts Discussed in Thread: SN74LVC1G07 Tool/software: Hi,
I gave +5V to supply pin.
Input of the channel = 5V.
when the control logic Low = 0V, I got 5V at the output of the channel/switch.
But when I changed the control…
Part Number: TS5A3167 Other Parts Discussed in Thread: TS5A3159A Are there any other active low SPST switches with the powered-off protection?
Regards,
JMMN
Part Number: TS5A3167 Other Parts Discussed in Thread: TMUX1511 , SN74CB3Q3125 , , TS5A23166 , TMUX1574 , TMUX1575 Hi There,
I am thinking use this part to isolate the signals between two power domain, battery (3.0V) and VCC-3.3V, the VCC may be powered…
Part Number: TS5A3167 Hi All,
Can you help to check what's the A1 pin position for TS5A3167 DSBGA package? We are confused for below two pictures in our datasheet:
Thanks.
Part Number: TS5A3167 Hello Team;
Our Customer pointing out that Outside Dimension of DSBGA are two different size, and would like to confirm these figure are correct or not? www.ti.com/.../scds187c.pdf
1) On top page, "Device information" Dody side…
Part Number: TS5A3167 Other Parts Discussed in Thread: TS5A3166 , , TMUX1574 Hello,
I found this E2E post that talks about the TS5A3166: e2e.ti.com/.../660359
The applications engineer mentioned the powered-off protection works properly when V+ is…