Part Number: TS5A1066 Other Parts Discussed in Thread: TS5A4624 , , TS5A3166 , TS5A3167 Hi team,
Does TS5A1066 support Isolation in Power-Down Mode as well as TS5A4624?
(i.e. Does COM or NO accept 3.3V when V+=0V?)
Best regards,
Itoh
Hi Kawsar,
I support the BQ25570 not the TS5A4624. If you remove the switch and connect the DAC (I'm assuming the 80% at NC) directly to VOC_SAMP, do you get the result that you want? Is VOC_SAMP floating or is the resistor divider there. I am not certain…
Hello Team, Thank you for your reply. I am planning to use the analog switch TS5A4624 . The control voltage at the pin IN will be 3.3V logic. The V+ pin will be powered from a 5V supply and the input signal to the COM pin will be between 0-5V and the…
Part Number: TS5A6542 Other Parts Discussed in Thread: TS5A4624 , TS5A9411
Hi team,
I need to select a 2:1 SPDT and 1 channel switch. Temperature is -40 to 85 and it will be OK. 90MHZ or 100MHZ bandwidth will be OK. The input signal is the current…
Puchong,
You can search for signal switches using the ti.com switch search tool . Select the filters for configuration 2:1, channel = 1, Vdd > 5V and I/O continuous current > 200mA. The TS5A12301E has lowest Ron in BGA package and TS5A4624 is in an…
Hi, Thank you for your question.
First, could you confirm which voltage specification the 1.8V specification is referring to? Is it the voltage supply, voltage of the signal passing through, or the logic level of the select/enable pin? We have switches…