Hi Lei,
I think Nir's equations are correct but the value he used for Vs was much higher than your application it seems, if you Vs is 0.35V, your equations are correct and the peak voltage is 1.425 V. That should be ok as long as the VDD > 1.425V.…
Part Number: TS5MP645 Hello team,
Is there any return loss characteristic for TS5MP645?
There is insertion loss, but I couldn't find return loss on the datasheet.
Best Regards, Kei Kuwahare
Part Number: TS5MP645 Other Parts Discussed in Thread: TMUX646 , TS5MP646 When I check the BW (Differential Bandwidth) specification of TS5MP645, it is listed as MIN: 1.5GHz, Typ: 2GHz, but is it possible to accept 1.3Gbps MIPI signal?
Part Number: TS5MP645 Hello. In the datasheet and the product landing webpage, there are 2 versions of this component listed.
TS5MP645YFPR
TS5MP645 N YFPR
What is the difference between the above 2 versions? Thanks.
Part Number: TS5MP645 Other Parts Discussed in Thread: TMUX646 Hi,
We have using the MIPI switch as like in the below image.
We facing Frame drop during the camera streaming in the CSI 1 port only , there is a stub in our board on CSI 1 data pairs .
…
Part Number: TS5MP645 hello team, Please help if you know. I would like to switch high-speed data of 10ch or more using multiple TS5MP645s. I would like to estimate the part to part skew in that case. But it's not mentioned in the specs. As an estimation…
Part Number: TS5MP645 Other Parts Discussed in Thread: TMUX646 , TS5MP646 , SN3257-Q1 Hi team,
we need 2:1 DSI mux on automotive application,
do we have Q product for automotive?
or other suitable part that have Q version.
Part Number: TS5MP645 Other Parts Discussed in Thread: TMUX646 Hi Team,
Good day!
Could you please help our customer? They are looking to create a raspberry pi based device with the ability to multiplex through 8 cameras. The cameras use CSI2, so as planned…