Part Number: TS5V330C Other Parts Discussed in Thread: TS5V330 Hello,
Regarding to the AC coupling capacitor on TS5V330C, my customer is asking a question.
(Question)
・They will use it on output (Dx) of TS5V330C.
Is it supported ? and is there any problem…
Kaitlyn,
I went to the TI.com switches and multiplexers selection tool and used the filters on the left hand side to input your criteria. It came back with 2 switches TS5L100 and TS5V330. I would look at using the TS5V330 since it comes in a 3.5mm x 4…
Praveen,
I used the signal switches selection tool on TI.com and filtered on your parameters.
1:2 SPDT Mux/Demux, Bidirectional
1.8V, 50 MHz Signal
4 Channel
Ron as low as possible
Package: TSSOP
The tool returned the below 7 devices. What do you think…
Other Parts Discussed in Thread: SN74CB3Q3257 , TS5A22362 , TS5V330 Hi,
Pls, suggest suitable audio and mic source select switch IC for call box application. signal voltage level Max. 5V only
SPDT Audio Switch 4-Channel 2:1 with one control
Thanks
Panne…